imx8mp evk - " no remote pad found " issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp evk - " no remote pad found " issue

102 Views
deevia
Contributor II

Hello NXP community,

I'm using imx8mp evk and OS:Yocto with LF6.6.3_1.0.0 bsp version.

I added a new layer and recipe for simple basic python application for reading camera(ov5640 connected via mipi csi) output and display it. Following is the python code

import gi

gi.require_version('Gst', '1.0')
from gi.repository import Gst

def play_video():
 
Gst.init(None)
source = Gst.ElementFactory.make("v4l2src", "source")
convert = Gst.ElementFactory.make("videoconvert", "convert")
sink = Gst.ElementFactory.make("autovideosink", "sink")
source.set_property("device", "/dev/video3")
pipeline = Gst.Pipeline.new("video-pipeline")
pipeline.add(source)
pipeline.add(convert)
pipeline.add(sink)

if not source.link(convert):
print("Source and convert could not be linked.")
return
 
if not convert.link(sink):
print("Convert and sink could not be linked.")
return

pipeline.set_state(Gst.State.PLAYING)
bus = pipeline.get_bus()
pipeline.set_state(Gst.State.NULL)
play_video()
 
got the following on console:
 
root@imx8mp-lpddr4-evk:/usr/bin# python3 ov5640_pythonapp.py
[   39.653787] mxc-mipi-csi2.0: mipi_csis_imx8mp_phy_reset, No remote pad found!
[   40.340239] mxc-mipi-csi2.0: mipi_csis_imx8mp_phy_reset, No remote pad found!
 
 
Could anyone please let me know what's issue or what i'm missing here,
My target is to read camera feed each image read time and also display the feed.
 
Thanks in advance,
 
Regards,
Deevia
0 Kudos
2 Replies

68 Views
joanxie
NXP TechSupport
NXP TechSupport

could you open ov5640 by gstreamera successfully with current bsp? did you change any kernel source code?

63 Views
deevia
Contributor II

Hello @joanxie ,

Thanks for reply, Yes I could open ov5640 via gstreamer and for mipi csi 2 i changed dts configuration like power down and reset pins so that i could see feed, but now i'm trying a basic python application for reading and displaying camera feed but i'm not able to acheive. I'm also try changing my application and try to make it work.

0 Kudos