imx8 is compatible with two AHD conversion chips

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8 is compatible with two AHD conversion chips

1,498 Views
songhongliang
Contributor II

hi,

I want use AHD chip, nvp6324 or tp2815, In imx8 mipi csi0,How to configure the device tree。

/*add by shl*/
#if 1
&i2c_mipi_csi0 {
#address-cells = <1>;
#size-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c_mipi_csi0>;
clock-frequency = <100000>;
status = "okay";

//7bit addr
nvp6324_mipi@30 {
compatible = "nextchip,nvp6324_mipi";
reg = <0x30>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_mipi_csi0>;
clocks = <&clk_dummy>;
clock-names = "capture_mclk";
mclk = <27000000>;
mclk_source = <0>;
virtual-channel;
pwn-gpios = <&lsio_gpio3 8 GPIO_ACTIVE_HIGH>;
status = "okay";

port {
nvp6324_0_ep: endpoint {
remote-endpoint = <&mipi_csi0_ep>;
data-lanes = <1 2 3 4>;
};
};
};

//7bit addr
tp2815_mipi@44 {
compatible = "techpoint,tp2815_mipi";
reg = <0x44>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_mipi_csi0>;
clocks = <&clk_dummy>;
clock-names = "capture_mclk";
mclk = <27000000>;
mclk_source = <0>;
virtual-channel;
irq-gpios = <&lsio_gpio3 7 GPIO_ACTIVE_HIGH>;
pwn-gpios = <&lsio_gpio3 8 GPIO_ACTIVE_HIGH>;
status = "disabled";

port {
tp2815_0_ep: endpoint {
remote-endpoint = <&mipi_csi0_ep>;
data-lanes = <1 2 3 4>;
};
};
};
/delete-node/ max9286_mipi@6a;
};

&mipi_csi_0 {
#address-cells = <1>;
#size-cells = <0>;
virtual-channel;
status = "okay";

/* Camera 0 MIPI CSI-2 (CSIS0) tp2815_0_ep nvp6324_0_ep*/
port@0 {
reg = <0>;
mipi_csi0_ep: endpoint {
remote-endpoint = <&nvp6324_0_ep>;
data-lanes = <1 2 3 4>;
};
};

/*
port@1 {
reg = <1>;
mipi_csi0_ep: endpoint {
remote-endpoint = <&nvp6324_0_ep>;
data-lanes = <1 2 3 4>;
};
};
*/
};
#endif

 

Thanks

0 Kudos
Reply
2 Replies

1,487 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

1,472 Views
songhongliang
Contributor II

HI

 What I mean is that it is compatible with tp2815 and nvp6324 on CSI0. In fact, only one chip is used at a time. With a mirroring code, it can be compatible with two chips and automatically identify and load the driver.

thanks

0 Kudos
Reply