Hi All,
I am trying to flash the iMX8QXP MEK board SPI memory with the SCU FW and U-Boot but when I try to use the command
sudo uuu -v -b qspi flash_uboot.bin flash_scfw.bin
or the same command for prebuilt images downloaded from NXP website. I get the "Fail HID(W):LIBUSB_ERROR_IO" error. Also, on checking the dmesg when running the UUU commands I can see that the USB type C port connected to the J11 port of the board is continuously disconnecting and reconnecting continuously. Can anyone suggest a fix for this issue?
Thanks and Regards,
Ramprakash
已解决! 转到解答。
Hello,
Yes, please find Linux BSP documentation here:
https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...
L5.4.70_2.3.0 yocto guide
i.MX Yocto Project User’s Guide
Best regards,
Aldo.
Hello,
Could you help me with the following questions:
Does this issue happen even if trying to flash another of the images in the prebuilt package?
i.e. flashing eMMC or SD card
Could you tell me if you're using a B0 or C0 chip?
Also, please share how you're creating the SPI image.
Best regards,
Aldo.
Hi @AldoG ,
Thanks for the reply. I now figured out that the issue does not happen with the prebuilt demo image. I used "imx-boot-imx8qxpc0mek-sd.bin-flash". But when I try to use the image which I built using mkimage tool the issue still occurs.
Thanks and Regards,
Ramprakash
Hello,
Thank you for checking, could you please share the steps you have follow to create your image using the mkimage?
Please note that if you have C0 chip you'll need to select this revision when building using mkimage.
Regards,
Aldo.
Hi @AldoG ,
Thanks for the reply.
I did try the REV=C0 with mkimage tool. But when I use the REV = C0 the command which gets executed still shows B0. And the image fails to flash SPI memory.
But when I try to hardcode the REV=C0 into the soc.mak file under iMX8QX folder I get a error that the Rev = C0 is not known. Do you have any idea how to fix this?
Thanks and Regards,
Ramprakash
Hello,
On my side I'm having different results, may I ask if you have downloaded the imx-mkimage form our git?
https://source.codeaurora.org/external/imx/imx-mkimage/tree/?h=imx_5.4.70_2.3.0
If not please try with these one, let me know if you see the same result.
Best regards,
Aldo.
Hi @AldoG ,
I now got the mkimage from the latest branch and built the SCU port, SECO, ATF and Uboot from the latest branch as well. I am now able to boot the SPI flash memory. But I get the following screen after the boot process starts. I am not able to enter any commands after it.
Hello,
From the log it looks correct, the boot process is not able to find a valid kernel since uboot was the only thing flashed, so it will switch to booting from net.
if you want to stop at uboot level, you'll need to stop the autoboot, this be typing any key in the serial console.
Regards,
Aldo.
Hi @AldoG ,
Thanks for the update. I am able to use the command line interface of u-boot after booting from SPI flash memory. I am now trying to build linux image using yocto. Can you share any material on how to build the rootfs and device tree buffers?
Thanks and Regards,
Ramprakash
Hello,
Yes, please find Linux BSP documentation here:
https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...
L5.4.70_2.3.0 yocto guide
i.MX Yocto Project User’s Guide
Best regards,
Aldo.