imx6sabrelite OCOTP_CFG0, OCOTP_CFG1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6sabrelite OCOTP_CFG0, OCOTP_CFG1

903 Views
myungjinhwang
Contributor III

dear freescale team

i have imx6sabrelite board and want to read device unique ID (OCOTP_CFG0, OCOTP_CFG1).

OCOTP_LOCK_TESTER[1] bit is set to 0 as bellow.

pastedImage_3.png

pastedImage_5.png

Q1.  fuse box is in security block on the block diagram. it could be read in non-secure mode ?

Q2. Can i read OCOTP_CFG0, OCOTP_CFG1 in the linux kernel or u-boot  c code with physical address without memtool utility?

Best regards,

0 Kudos
1 Reply

511 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Please look at the following

How to read i.MX6DQ unique ID.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos