imx6dualite and micron DDR3 bringup issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6dualite and micron DDR3 bringup issue

683 Views
pavithraravi
Contributor I

Hi

 

we are using following parts and facing issue in ddr bringup.

1. processor - imx6dualite

2. DDR - micron - MT41K256M16TW-107 IT

 

Note: USB OTG is not available on our custom board. Boot mode is set to SD card boot.

 

Here we have attached the DDR script and configuration used.

We would like to know whether we are missing anything important.

Original Attachment has been moved to: eliuaccs6sdl_tmp.cfg.zip

Labels (1)
Tags (2)
0 Kudos
1 Reply

468 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the following documents how to configure DDR parameters.

 

https://community.nxp.com/docs/DOC-101708 

 i.MX6 DDR Register Programming Aids 

 

  Note, timing parameters for the MT41K256M16TW should be set,

assuming that i.MX6 memory frequency is 532 MHz, that is memory

parameters for Data Rate of 1066 should be used.

  For example tRCD=tRP=CL (ns) in Your table is 13.75 ns, it may be

recommended - 13.1 ns (really Your settings should not provide problems).

 tRC = 39 ns in the case, but it would be better to apply 52.5 ns.

 

You selected DRAM Clock Freq (MHz) of 400 MHz, this means DDR3-800

specs should be applied.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos