hi nxp
I use kernel linux-4.9.11, however, The color of different of lvds screens output is not same, I want to adjust the colour characteristics to allow for differences in the behaviour of the lcd panels so that the colours appear the same on both screens.?
You can take a picture for the different color LVDSs display. You also can send us your boot log file.
this is same picture, but display differently on different lvds panel:
this is cold color
warm colour:
i want to adjust second picture to slightly blue, how I can do ?
You can not realize it, for the different LVDSs, it's normal to see different color. Because for the different LVDSs screen the timings are different . So you can the above not same color displays.
it means that the same picture output on different LVDS display have different color?
Yes, they have different timing, it's normal.
Android or linux BSP are you using? Which version? Is your board you designed or NXP reference board?
hi Rita Wang I use yocto L4.9.11_1.0.0 on i.MX6dlsabread soc