imx6 DDR Stress Test Restart -- Watchdog?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 DDR Stress Test Restart -- Watchdog?

884件の閲覧回数
batwings
Contributor II

I see that my device is resetting at 128s once I execute the DDR Stress Test file :   ddr-test-uboot-jtag-mx6dl.bin

Which I believe is caused by the watchdog timer not being serviced since 128s is the max for the imx6 watchdog timer.

 Using the uboot option (Option 3) here:

i.MX6/7 DDR Stress Test Tool V3.00 

 

We are using an extended temperature imx6

CPU: Freescale i.MX6SOLO rev1.2 996 MHz (running at 792 MHz)
CPU: Extended Commercial temperature grade (-20C to 105C) at 35C

In uboot the code turns off the watchdog, is there a way to check that in Uboot?   I can wait sit in Uboot many minutes without executing a command and not get a restart.  But once I execute the go instruction to start the DDR Stress Test code, the device always resets after 128s.   It does not matter if I run the Calibration Test first or if I skip it and go straight to the Stress test.    Always get a reset after 128s.

Is the watchdog getting enabled in the Stress test?    What can I look at to see if its the watchdog?

Commands:

=> icache off
=> dcache off

=> ext4load mmc 0:1 0x907000 /ddr-test-uboot-jtag-mx6dl.bin
71812 bytes read in 161 ms (435.5 KiB/s)
=> go 0x907000
## Starting application at 0x00907000 ...

<<<<<   128s later device will reboot, operation does not matter >>>>

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

760件の閲覧回数
batwings
Contributor II

Hi Igor,

     I checked that WDE is set to 0 and we are using Boot mode[1:0] of 10 (Internal Boot).  So the Serial Downloader setting the watchdog does not apply.

0 件の賞賛
返信

760件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jason

I do not think that watchdog is enabled in the ddr test.

One can check bit WDE(Watchdog Enable) register WDOG_WCR described in

sect.70.7.1 Watchdog Control Register (WDOGx_WCR)

i.MX 6Solo/6DualLite Applications Processor Reference Manual

also from sect.8.2.4 Serial Downloader :

"In this mode, the ROM programs the WDOG1 for a 90-second time-out if the
WDOG_ENABLE eFuse is 1"

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信