imx28 clock inaccuracy

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx28 clock inaccuracy

1,566件の閲覧回数
nizamkhatri
Contributor I

We have a unique problem with imx28 clock accuracy in our design.

 

The 32.768 kHz crystal is connected to the RTC and is battery-backed.  There is also a 24MHz crystal that runs the system clock when powered by the 5V supply.  In our case, we found that the RTC when running on battery is more accurate (within 20ppm) than when it is powered by the 5V supply.  Additionally, we found that the 24MHz clock is more accurate (within 20ppm) than the 32.768 kHz clock when powered by the 5V supply.  Therefore, in order to be within 20ppm in all cases, during initial power up to the 5V supply, we copy the contents of RTC clock to the 24MHz system clock, and when detecting loss of 5V during power down, we copy the contents of the system clock to the battery-backed RTC before shutting down the CPU.

During power cycle tests, we are seeing somewhat random occurrences of inaccuracies from seconds to minutes in the system clock.  Thus far, we have been unable to find the source of the problem in our code.  We also do not think it is due to the hardware implementation of the battery back circuit as shown below.

Let us know if you may have run into a similar issue and found a fix or if you have other suggestions or ideas that we could try.    

pastedImage_1.png        

ラベル(2)
0 件の賞賛
返信
1 返信

1,450件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nizam

if 24MHz clock is more accurate than 32.768 kHz clock, then this

may point to instable 32.768 kHz crystal operation due to noise from power supplies or emi.

One can try to test with external 32.768 kHz clock or reproduce this issue on i.MX28 EVK

reference board.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信