imx-yocto-L5.15.5_1.0.0​ BSP startup issue on iMX6Q board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx-yocto-L5.15.5_1.0.0​ BSP startup issue on iMX6Q board

897件の閲覧回数
caritzhu
Contributor III

First of all, our iMX6Q board could be work properly under imx-yocto-L4.9.88_2.0.0 BSP by using X11 backend. However, I found a startup issue when I want to update BSP to imx-yocto-L5.15.5_1.0.0​ which is your latest linux release BSP. BTW, I use the command "DISTRO=fsl-imx-wayland MACHINE=imx6qsabresd source imx-setup-release.sh -b build-wayland" to setup the enviroment, then use the command "bitbake imx-image-multimedia" to compile the Yocto system image. Unfortunately, we fount that the u-boot and kernel is startup noramlly and we could see the "penguin" logo and "openembedded" boot screen, but after that the weston destop could not be displayed properly which looks like "blurred screen".

The log and video are in the attachment.

0 件の賞賛
返信
3 返答(返信)

857件の閲覧回数
caritzhu
Contributor III

Hello, anyone could help me or give me some suggestions?

0 件の賞賛
返信

886件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello caritzhu,

 

Do you compile and build the image? try again to burn it, erase everything in the sd or emmc and burn again.

Regards

0 件の賞賛
返信

883件の閲覧回数
caritzhu
Contributor III

Hello,

 

Yes, I have reburn for several times and even changed to build xwayland image and the situation is the same. Do I need to change some configuration in weston.ini? My board only support to display by LVDS.

0 件の賞賛
返信