imx_usb 2184200.usb: 2184200.usb supply vbus not found, using dummy regulator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx_usb 2184200.usb: 2184200.usb supply vbus not found, using dummy regulator

1,754件の閲覧回数
jupiter_hce
Contributor III

Hi,

I am running a custom iMX6ULZ, I am concerning imx_usb error that  vbus not found, using dummy regulator? I've read the i.MX_Linux_Reference_Manual.pdf and enabled following configure as per 39.3.3 Menu Configuration Options., what I could miss?

CONFIG_USB_NET_DRIVERS=y

CONFIG_USB_EHCI_HCD=y

CONFIG_USB_CHIPIDEA=y

CONFIG_USB_CHIPIDEA_UDC=y

CONFIG_USB_CHIPIDEA_HOST=y

CONFIG_USB_GADGET=y

CONFIG_USB_MXS_PHY=y

I don't see anything I might miss, do I? I don't think to change loadable module support would fix it, but I could be wrong.

Thank you.

Kind regards,

jh

 

 

 

 

0 件の賞賛
返信
1 返信

1,744件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jupiter

 

what bsp used in the case, may be recommended to try one from source.codeaurora.org/external/imx/linux-imx repository

for 2184200.usb one can look at

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ul.dtsi?h=lf-5.10.y

 

Best regards
igor

0 件の賞賛
返信