iMX8DXL EVK eMMC flashing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8DXL EVK eMMC flashing

983 Views
sheik
Contributor I

Hi,

I am trying to flash iMX8DXL EVK's eMMC using uuu tool.

I have downloaded uuu binary from this link https://github.com/NXPmicro/mfgtools/releases/tag/uuu_1.3.130

I have taken the binaries from L5.4.70-2.3.0_images_MX8DXLEVK release.

According to iMX Linux User Guide section 4.2.2, I am trying to flash the eMMC using below command,

sudo ./uuu -V -b emmc_all imx-boot-imx8dxlevk-sd.bin-flash imx-image-multimedia-imx8dxlevk.wic

I have removed standard SD card so that EVK will go to serial download mode. USB OTG is getting detected but flashing get stuck in first step itself.

Please check the below log prints.

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.126-0-gb77f1b8

Build in config:
Pctl Chip Vid Pid BcdVersion
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDPS: MX8DXL 0x1fc9 0x0147
SDPS: MX28 0x15a2 0x004f
SDPS: MX815 0x1fc9 0x013e
SDPS: MX865 0x1fc9 0x0146
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02

Run built-in script:

uuu_version 1.2.39

# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f imx-boot-imx8dxlevk-sd.bin-flash

# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM
SDPS: boot -f imx-boot-imx8dxlevk-sd.bin-flash

# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f imx-boot-imx8dxlevk-sd.bin-flash -offset 0x57c00
SDPU: jump
# }

# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f imx-boot-imx8dxlevk-sd.bin-flash -skipspl
SDPV: jump
# }


FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}
FB: ucmd mmc dev ${emmc_dev}
FB: flash -raw2sparse all imx-image-multimedia-imx8dxlevk.wic
FB: flash bootloader imx-boot-imx8dxlevk-sd.bin-flash
FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;
FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
FB: done


Wait for Known USB Device Appear...
libusb: error [udev_hotplug_event] ignoring udev action bind
New USB Device Attached at 1:1
1:1>Start Cmd:SDPS: boot -f imx-boot-imx8dxlevk-sd.bin-flash
100%1:1>Okay (2.031s)

Please let me know if I am missing something asap.

Regards,

Sheik Ajith

0 Kudos
Reply
1 Reply

946 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Please Download UUU version 1.3.130 or later from https://github.com/NXPmicro/mfgtools/releases. After uuu_1.3.130 version add i.MX8DXL support. If still not work tell us.

0 Kudos
Reply