iMX6 sabre board MfgTool2 not working.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 sabre board MfgTool2 not working.

2,636 Views
sudhirdumbhare
Contributor I

Hi,

Trying to flash iMX6 sabre board by using MfgTool2(with fresh SD card), but it is not working, Am refering "Manufacturing Tool V2 Quick Start Guide",IMX6SABREINFOQSG.pdf document. MfgTool2 is stop after "ModuleID[2] LevelID[10]: ExecuteCommand--Push[WndIndex:0], Body is $ mknod block,mmcblk0,/dev/mmcblk0,block ModuleID[2] LevelID[1]: PortMgrDlg(0)--MSCDevice--Command Push(no file) excute failed" Any help is appreciable. Thanks in advanced.

1) MfgTool version : Mfgtools-Rel-13.01.00_ER_MX6Q_UPDATER.

2) Attached is mfgtool2 cfg,UIcfg & mfgtool log.

Original Attachment has been moved to: MfgTool.log.zip

Original Attachment has been moved to: UICfg.ini.zip

Original Attachment has been moved to: cfg.ini.zip

Labels (1)
0 Kudos
3 Replies

1,089 Views
igorpadykov
NXP Employee
NXP Employee

Hi sudhir

please use latest MFG Tool,

one can try with default images

IMX_6DQ_MFG_TOOL

also verify that SD inserted in SD3 slot. One can try with

another SD card (also check SD write protection slider).

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,089 Views
sudhirdumbhare
Contributor I

Thanks for reply.

As per document (SABRE for Automotive Infotainment Based on th|Freescale

IMX6SABREINFOQSG.pdf ), on page no 4 & 5, there are only two sd card slot. Not seen

3rd SD slot. Could you provide more details on that.

DIP Switch Configurations set as per Table 3: Boot Configuration DIP Switches(page 10) &

Table 4: Boot Mode DIP Switches (page 11).

Also am tried with IMX_6DQ_MFG_TOOL , but no luck :smileysad:.

Am checking with serial terminal with the given serial port settings ( also tried with

different combination)Just got junk character. Did I missed any setting?

Regards,

Sudhir

0 Kudos

1,089 Views
igorpadykov
NXP Employee
NXP Employee

"SD3 slot" was meant not number of SD connectors but

SD interface number. For numbering one can look

at IMX6SDLRM i.MX 6Solo/6DualLite Applications Processor Reference Manual

Please confirm, what board and processor are you using:

i.MX6Q,i.MX6D,i.MX6S,i.MX6DL,i.MX6SoloLite.

Also I attached presentation which gives general picture of i.MX6

development, please read starting from p.30.

Best regards

chip

0 Kudos