iMX6 Sabreai Auto Eval Board login failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 Sabreai Auto Eval Board login failed

1,027 Views
shijiaguo
Contributor II

Hello,

I have an iMX6 sabreai quad automotive eval board. I've built the kernel with an console only image. I downloaded the image to SD card and it booted ok. I can log in with just the username root. However today I was trying to boot with NFS, and ever since I configured that, I log in with root, yet it prompted me with a password request. What do I put in for this password? Any idea?

Here's my uboot config:

baudrate=115200                                                            
boot_fdt=try                                                               

bootargs=console=${console},${baudrate} ${smp} root=/dev/nfs ip=dhcp nfsroot=${se

rverip}:${nfsroot},v3,tcp                                                  
bootcmd=run netboot                                                   

bootcmd-ori=mmc dev ${mmcdev};if mmc rescan; then if run loadbootscript; then run

bootscript; else if run loadimage; then run mmcboot; else run netboot; fi; fi; e

lse run netboot; fi                                                        
bootcmd_mfg=run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr}; 
bootdelay=1                                                                
bootfile=zImage                                                            
bootscript=echo Running bootscript from mmc ...; source                    
console=ttymxc3                                                            
emmcdev=2                                                                  
epdc_waveform=epdc_splash.bin                                              
ethact=FEC                                                                 
ethaddr=00:04:9f:04:42:e4                                                  
ethprime=FEC                                                               
fdt_addr=0x18000000                                                        
fdt_file=imx6q-sabreauto.dtb                                               
fdt_high=0xffffffff                                                        
fileaddr=18000000                                                          
filesize=b744                                                              
gatewayip=10.75.50.1                                                       
image=zImage                                                               
initrd_addr=0x12C00000                                                     
initrd_high=0xffffffff                                                     
ip_dyn=no                                                                  
ipaddr=10.75.50.157                                                        
loadaddr=0x12000000                                                        
loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};     
loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}           
loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}            

mfgtool_args=setenv bootargs console=ttymxc3,115200 rdinit=/linuxrc g_mass_storag

e.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1

g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iS

erialNumber="" enable_wait_mode=off                                        

mmcargs=setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot}   

mmcautodetect=yes                                                          

mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test

${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdt_addr}; el

se if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi;

fi; else bootz; fi;                                                       
mmcdev=1                                                                   
mmcpart=1                                                                  
mmcroot=/dev/mmcblk2p2 rootwait rw                                         

netargs=setenv bootargs console=ttymxc3,115200  root=/dev/nfs ip=10.75.50.157 nfs

root=10.75.50.151:/opt/iMX6,v3,tcp                                         

netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then set

env get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${bo

ot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_fil

e}; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bo

otz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;           
netmask=255.255.255.0                                                      
nfsroot=/opt/iMX6                                                          
script=boot.scr                                                            
serverip=10.75.50.151                                                      

tftpbootcmd=tftpboot ${loadaddr} ${bootfile}; tftpboot ${fdt_addr} ${fdt_file}; r

un mmcargs; bootz ${loadaddr} - ${fdt_addr};                               

here's the last few messages before it prompted me to log in:

fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_ad

dr=2188000.ethernet:01, irq=-1)                                                 

IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready                              

fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx       

IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready                         

IP-Config: Guessing netmask 255.0.0.0                                           

IP-Config: Complete:                                                            

     device=eth0, hwaddr=00:04:9f:04:42:e4, ipaddr=10.75.50.157, mask=255.0.0.0,

gw=255.255.255.255                                                              

     host=10.75.50.157, domain=, nis-domain=(none)                              

     bootserver=255.255.255.255, rootserver=10.75.50.151, rootpath=             

can-stby: disabling                                                             

can-en: disabling                                                               

usb_otg_vbus: disabling                                                         

SW4: disabling                                                                  

ALSA device list:                                                               

  #0: cs42888-audio                                                             

  #1: imx-spdif                                                                 

  #2: imx-hdmi-soc                                                              

VFS: Mounted root (nfs filesystem) readonly on device 0:14.                     

devtmpfs: mounted                                                               

Freeing unused kernel memory: 428K (80a8f000 - 80afa000)                        

INIT: version 2.88 booting                                                      

Starting udev                                                                   

udevd[203]: starting version 182                                                

DBG sensor data is at 7f0141c0                                                  

random: nonblocking pool is initialized                                         

ERROR: v4l2 capture: slave not found!                                           

bootlogd: cannot allocate pseudo tty: No such file or directory                 

urandom start: failed.                                                          

Populating dev cache                                                            

/etc/rcS.d/S36udev-cache: line 67: /etc/udev-cache.tar.gz: Permission denied    

udev-cache: update failed!                                                      

/etc/rcS.d/S37populate-volatile.sh: line 56: /etc/volatile.cache.build: Permissio

n denied                                                                        

rm: can't remove '/etc/udev/cache.data': Permission denied                      

/etc/rcS.d/S37populate-volatile.sh: line 56: /etc/volatile.cache.build: Permissio

n denied                                                                        

/etc/rcS.d/S37populate-volatile.sh: line 56: /etc/volatile.cache.build: Permissio

n denied                                                                        

/etc/rcS.d/S37populate-volatile.sh: line 86: /etc/volatile.cache.build: Permissio

n denied                                                                        

/etc/rcS.d/S37populate-volatile.sh: line 86: /etc/volatile.cache.build: Permissio

n denied                                                                        

/etc/rcS.d/S37populate-volatile.sh: line 86: /etc/volatile.cache.build: Permissio

n denied                                                                        

/etc/rcS.d/S37populate-volatile.sh: line 86: /etc/volatile.cache.build: Permissio

n denied                                                                        

/etc/rcS.d/S37populate-volatile.sh: line 86: /etc/volatile.cache.build: Permissio

n denied                                                                        

/etc/rcS.d/S37populate-volatile.sh: line 56: /etc/volatile.cache.build: Permissio

n denied                                                                        

/etc/rcS.d/S37populate-volatile.sh: line 33: /etc/volatile.cache.build: Permissio

n denied                                                                        

/etc/rcS.d/S37populate-volatile.sh: line 33: /etc/volatile.cache.build: Permissio

n denied                                                                        

/etc/rcS.d/S37populate-volatile.sh: line 86: /etc/volatile.cache.build: Permissio

n denied                                                                        

ln: /etc/resolv.conf: Permission denied                                         

/etc/rcS.d/S37populate-volatile.sh: line 33: /etc/volatile.cache.build: Permissio

n denied                                                                        

/etc/rcS.d/S37populate-volatile.sh: line 33: /etc/volatile.cache.build: Permissio

n denied                                                                        

/etc/rcS.d/S37populate-volatile.sh: line 56: /etc/volatile.cache.build: Permissio

n denied                                                                        

/etc/rcS.d/S37populate-volatile.sh: line 56: /etc/volatile.cache.build: Permissio

n denied                                                                        

ALSA: Restoring mixer settings...                                               

No state is present for card imxspdif                                           

Found hardware: "imx-spdif" "" "" "" ""                                         

Hardware is initialized using a generic method                                  

No state is present for card imxspdif                                           

INIT: Entering runlevel: 5                                                      

Configuring network interfaces... ifup skipped for nfsroot interface eth0       

run-parts: /etc/network/if-pre-up.d/nfsroot exited with code 1                  

Could not create /var/lib/dbus/machine-id.GwziGoJf: Permission denied           

Starting system message bus: dbus.                                              

Starting rpcbind daemon...done.                                                 

Starting advanced power management daemon: No APM support in kernel             

(failed.)                                                                       

Starting syslogd/klogd: done                                                    

* Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon                              

   ...done.                                                                     

Starting Telephony daemon                                                       

Starting Linux NFC daemon                                                       

                                                                                

Freescale i.MX Release Distro 4.1.15-1.1.1 imx6qsabreauto /dev/ttymxc3          

                                                                                

imx6qsabreauto login: root                                                      

Password:                                                                       

Login incorrect                                                                 

                                                                                

imx6qsabreauto login:

Labels (3)
0 Kudos
Reply
1 Reply

644 Views
b36401
NXP Employee
NXP Employee

Please try to set empty password for root:

root@tecno:~# head -1 /media/040d5655-7d9f-4913-8594-b5540c0fe51a/etc/passwd

root::0:0:root:/home/root:/bin/sh

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply