iMX6 SDR12 Suport

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 SDR12 Suport

892件の閲覧回数
johnjohntobias
Contributor II

Hello All,

I have a new iMX6SL custom board with WiLink8 chipset. The chipset has some features of SDIO 3.0 support and the I/O is 1.8v or (SDR25). I used the

mainline kernel 3.13, 3.19 and the Freescale (fsl-yocto-3.10.53-1.1.0), all of them detects the wifi. All of them uses 3.3v voltage signal.


clock:          50000000 Hz

actual clock:   49500000 Hz

vdd:            7 (1.65 - 1.95 V)

bus mode:       2 (push-pull)

chip select:    0 (don't care)

power mode:     2 (on)

bus width:      2 (4 bits)

timing spec:    2 (sd high-speed)

--->>> signal voltage: 0 (3.30 V)  <---> it should be 1.8v

I would like to know if there's any available patches out there that I

could use in order support SDR25?.

Regards,

John Tobias

ラベル(7)
0 件の賞賛
返信
2 返答(返信)

675件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi John

usually 1.8v selection is implemented by signal

x_VSELECT_SDx, such as in U508

i.MX6_SABRE_AI_DESIGNFILES   p.6  SPF-27142

Linux i.MX6SL has two board files mx6sl_arm2 (supported by ltib)

mx6sl_evk (supported by yocto and ltib). x_VSELECT_SDx is implemented

only on mx6sl_arm2 board.


Regarding sd3.0 support one can look below


linux-2.6-imx.git - Freescale i.MX Linux Tree


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

675件の閲覧回数
johnjohntobias
Contributor II

Hi Igor,

Thanks for the response. I got it working.

Regards,

John

0 件の賞賛
返信