iMX6 PCIe问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 PCIe问题

617 Views
feriaxue
Contributor I

Why is this?

iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.

CLK setup,by OpenEmbed---

CLK setup,by OpenEmbed

IMX PCIe pcie_rst, 0.

IMX PCIe pcie_rst, 1.

PCIE: imx_pcie_pltfm_probe start link up.

link up failed, DB_R0:0x004a4a02, DB_R1:0x08000000!

IMX PCIe port: link down!

Labels (2)
0 Kudos
Reply
1 Reply

387 Views
igorpadykov
NXP Employee
NXP Employee

Hi Feria

please try patch fixing PCIe detection

 

http://git.denx.de/?p=u-boot.git;a=commitdiff;h=5a82e1a21d1229e7e3d1c64187735794019e9a1b

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply