i.mx6qsabresd android reboot problem?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6qsabresd android reboot problem?

3,560 Views
allen_kim1
Contributor I

Dear team,

My customer is using i.MX6Q for their board and OS android 5.0.0

They using nfs booting but  android immediately reboot

error 1

root@sabresd_6dq:/ # kill init: critical process 'servicemanager' exited 4 times in 4 minutes; rebooting into recovery mode

SysRq : Emergency Remount R/O

EXT4-fs (mmcblk3p4): re-mounted. Opts: (null)

EXT4-fs (mmcblk3p6): re-mounted. Opts: (null)

Emergency Remount complete

imx2-wdt 20c0000.wdog: Device shutdown: Expect reboot!

reboot: Restarting system with command 'recovery'

error 2

root@sabresd_6dq:/ # init: critical process 'healthd' exited 4 times in 4 minutes; rebooting into recovery mode

SysRq : Emergency Remount R/O

EXT4-fs (mmcblk3p4): re-mounted. Opts: (null)

EXT4-fs (mmcblk3p6): re-mounted. Opts: (null)

Emergency Remount complete

imx2-wdt 20c0000.wdog: Device shutdown: Expect reboot!

reboot: Restarting system with command 'recovery'

U-Boot 2014.04-00201-g9d7bf9b (May 04 2015 - 16:18:13)

What point do i check ?

Thanks, BR

Labels (2)
0 Kudos
4 Replies

2,340 Views
skaicai
Contributor I

​Plz check the file I have upload , include the bootargs and boot kernel log. plz help to check the reason for the adb reboot bootloader fail. This lead to fail boot into fastboot . Thanks !

0 Kudos

2,340 Views
aravinthkumarja
Senior Contributor II

Hi Allen kim,

It have many of reasons to facing this issue. Can you add entire bootlog and bootargs.

Thanks!

Aravinth

0 Kudos

2,340 Views
skaicai
Contributor I

I have this problem too,Is there any wrong with the adb reboot bootloader in IMX6Q ? I have the same kernel log, Is there any solution ?

0 Kudos

2,340 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aleen

seems incorrect bootargs were used, please check parameter "nfsroot"

in attached Android_User's_Guide.pdf sect. 6.3.2 Kernel command line (bootargs)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos