i.mx25 532mhz?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,066件の閲覧回数
PatrickLin
Contributor I

    Hi:
The FSL site below stated that mx25 can run up to 532mhz? It is true or just typo?

https://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX251

ラベル(1)
0 件の賞賛
返信
1 解決策
895件の閲覧回数
PatrickStilwell
NXP Employee
NXP Employee

Any of the ARM processors can be overclocked to take advantage of your particular use case.  However, the i.MX25 CPU spec is 400MHz.

On page 1 of the datasheet:

At the core of the i.MX25 is Freescale's fast,proven, power-efficient implementation of the

ARM926EJ-S core, with speeds of up to 400 MHz.


元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
896件の閲覧回数
PatrickStilwell
NXP Employee
NXP Employee

Any of the ARM processors can be overclocked to take advantage of your particular use case.  However, the i.MX25 CPU spec is 400MHz.

On page 1 of the datasheet:

At the core of the i.MX25 is Freescale's fast,proven, power-efficient implementation of the

ARM926EJ-S core, with speeds of up to 400 MHz.


0 件の賞賛
返信
895件の閲覧回数
Yuri
NXP Employee
NXP Employee

Strictly speaking the i.MX25  is qualified / tested for CPU frequencies up to 400 MHz.

0 件の賞賛
返信
895件の閲覧回数
Nouchi
Senior Contributor II

Hello,

It's seems that is possible to clock the core @532Mhz, but this ARM core only support 400MHz, it could work, .....or not

0 件の賞賛
返信