Hi,
I am trying to set up multicore communication using RPMsg in IMX8QXP, in which freertos is running in M4 core and linux in A35. I am using the 'rpmsg_lite_str_echo_rtos' example from NXP FreeRTOS SDK 2.3. I was successfully able to create virtual tty '/dev/RPMSG'. Also i was able to send data to M4 core using 'echo' command from linux, and readback the acknowledgement at A35.
Now i want to use this same channel to pass data from Linux continuously to M4 (and read the acknowledgements). What I am looking for, is a simple userspace application in c using basic open, read, write commands to pass data from A35 to M4.
I tried this and got the results below :
I also tried using fopen, fwrite, fflush, fread commands with same results.
I am only using the basic open, read write commands. Am i missing something here? Please help.
please revert back if you need any more details.
Regatds,
Ajmal
已解决! 转到解答。
Hi Ajmal
for simple rpmsg testing one can try unit-test and attached Linux Manual
sect.9.19 Remote Processor Messaging:
rpmsg\test - imx-test - i.MX Driver Test Application Software
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi ajmalali,
maybe i am offtopic but regarding to speed in RPMSG you can read thread here Increasing transfer speed between cores · Issue #20 · EmbeddedRPC/erpc · GitHub start with ablaylock answer.
Hi Ajmal
for simple rpmsg testing one can try unit-test and attached Linux Manual
sect.9.19 Remote Processor Messaging:
rpmsg\test - imx-test - i.MX Driver Test Application Software
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi, ajmalali,
how are your problems been solved ?
I'm using a imx7d board, i want to send a int value from m4 to a7 and read it at a7 side.
I also use open, write,read commands,
but, m4 side print junk message and a7 side get nothing, just in blocking.
could you give me some advice ?
Regards,
Yu
Hi Yu,
The above test program that igor shared worked for me. Have you tried that?
Have you figured out where the problem is? ie. M4 or A7 side?
Also, just for clarity are you using bare metal application in the m4 side or do you have FreeRTOS or something similar in M4 core?
I started from the RPMsg application from the SDK by NXP and it worked for me.
You can get the SDK from here,
Welcome | MCUXpresso SDK Builder
Regards,
Ajmal