i.MX8M-Mini definition of CCM_CLKO[2:1] pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M-Mini definition of CCM_CLKO[2:1] pins

800 Views
vincentz63
Contributor IV

Document IMX8MMRM-i.MX 8M Mini Applications Processor Reference Manual, Rev 1, 03/2019 states that CCM_CLKO[2:1] can be connected to pads GPIO1_IO[14:15] (p. 1231). The signals are shown on page 262 as coming out of the CCM.

However, I cannot find the description for CCM_CLKO[2:1]. Could you let me know what this signal is? I am hoping it may be a clock output from the SoC.

Thanks

JP

Labels (1)
Tags (2)
0 Kudos
2 Replies

690 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello JP,

The CCM_CLKO pins are indeed lacking documentation but while these refer to an output for clocks it is not recommended to drive external devices as CCM_CLKO is designed only for monitoring on this processor.

My apologies for the inconvenience and thank you for pointing out the lack of information on the documentation!

Regards,

0 Kudos

690 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello JP,

The CCM_CLKO signal does usually refer to a clock output for off-chip devices. However, I will escalate with our experts so they can confirm this and to add this information on the next release of the documentation.

 

Regards,

0 Kudos