Hi,
I used i.MX8QM platform and in camera driver changed "streamcap.timeperframe.denominator" this value to 15 or 60
but why use application get camera output frame rate always 30?
If I want to diff camera frame rate output,what need changed or i.MX8 lock it 30?
已解决! 转到解答。
Hi Xu
seems frame rate is defined in driver described in
Table 6-5. Omnivision V4L2 Camera Driver Files attached Linux Manual,
like "#define DEFAULT_FPS" in driver code:
ov5640_mipi_v3.c\imx8\platform\media\drivers - linux-imx - i.MX Linux kernel
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------