i.MX6ULL Compile Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6ULL Compile Error

2,922件の閲覧回数
ray_deng1
Contributor III

Dears,

  I did separate compiled for imx-yocto-LF_L5.4.3_1.0.0, and already downloaded all the required components, but when it show below error.

| make[2]: *** No rule to make target 'arch/arm/boot/dts/imx6ull-14x14-evk-usb-certi.dtb'.  Stop.

Attached the error log for your reference,

Thanks &BRs,

Ray

ラベル(1)
0 件の賞賛
7 返答(返信)

2,552件の閲覧回数
donoldham
Contributor I

I am have the same problem. Followed the procedure in the latest NXP yocto guide Rev. L5.4.24_2.1.0, 06/2020

$ mkdir imx-yocto-bsp
$ cd imx-yocto-bsp
$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest
-b imx-linux-zeus -m imx-5.4.24-2.1.0.xml
$ repo sync

DISTRO=fsl-imx-fb MACHINE=imx6ull14x14evk source imx-setup-release.sh -b build

bitbake core-image-minimal

I tried different images, but still get the error

"scripts/kconfig/conf --syncconfig Kconfig"

"make[2]: *** No rule to make target 'arch/arm/boot/dts/imx6ull-14x14-evk-usb-certi.dtb'. Stop"

".../build/tmp/work-shared/recipe for target 'imx6ull-14x14-evk-usb-certi.dtb' failed". 

0 件の賞賛

2,552件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for 6ull, try to use 5.4.3_1.0.0

0 件の賞賛

2,552件の閲覧回数
radhikasomaiya
Senior Contributor II

Hi ray.deng@avnet.com ,

From Table 1. i.MX Yocto project images of attached yocto project user's guide imx-image-full is not supported on i.MX6ULL. These images are only supported for i.MX SoC with hardware graphics, So you cannot build imx-image-full for i.MX6ULL.

Regards,

Radhika Somaiya. 

0 件の賞賛

2,552件の閲覧回数
ray_deng1
Contributor III

Hi Radhika,

Got it , thanks,

BRs,

Ray Deng

Field Application

South FAE,Avnet China

深圳市宝安区新安街道创业二路与留仙一路交汇处东侧创芯研发中心1栋5楼

5th Floor, Building 1, Wise R&D Center, Liuxian 1st Road cross Chuangye 2nd Road,69th Block, Boa ’an District,Shenzhen City

O +8675586342385

M +8618026960272

D +8675586342385

F +867558378.0826

avnet.com<https://emea01.safelinks.protection.outlook.com/?url=http%3A%2F%2Favnet.com%2F&data=02%7C01%7Cws.wong%40nxp.com%7Cb1694567060e40ace47208d59de6bc7d%7C686ea1d3bc2b4c6fa92cd99c5c301635%7C0%7C0%7C636588536688437382&sdata=%2ByRoHs0%2FqgD%2BDwbxAes4iThAy8ghHMQ1AaWisaRqYqs%3D&reserved=0>

发件人: radhika.somaiya@volansystech.com <admin@community.nxp.com>

发送时间: 2020年5月12日 14:19

收件人: Deng, Ray <Ray.Deng@AVNET.COM>

主题: Re: - Re: i.MX6ULL Compile Error

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: i.MX6ULL Compile Error

reply from Radhika Somaiya<https://community.nxp.com/people/radhika.somaiya@volansystech.com?et=watches.email.thread> in i.MX Processors - View the full discussion<https://community.nxp.com/message/1310405?commentID=1310405&et=watches.email.thread#comment-1310405>

0 件の賞賛

2,552件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what build commands do you use? pls share this, let me double check it

0 件の賞賛

2,552件の閲覧回数
radhikasomaiya
Senior Contributor II

Hi ray.deng@avnet.com ,

We are able to build with imx-yocto-LF_L5.4.3_1.0.0 for i.MX6ULL14x14evk. Our host system is ubuntu 16.04.

Our configurations are as per below:

     Distro : fsl-imx-wayland

     Machine : imx6ull14x14evk 

We have tried both images.

     Image 1 : core-image-minimal

     Image 2 : fsl-image-machine-test 

We have followed the steps from Yocto project User's guide.(You can download document's from below link).

https://www.nxp.com/webapp/Download?colCode=L5.4.3_1.0.0_LINUX_DOCS 

Can you please give us the steps which you have followed?

Regards,

Radhika Somaiya.

0 件の賞賛

2,552件の閲覧回数
ray_deng1
Contributor III

Hi Radhika,

Thanks for your response. I use below configurations,

Our configurations are as per below:

Distro : fsl-imx-fb

Machine : imx6ullevk

We have tried both images.

Image 1 : imx-image-full

BRs,

Ray Deng

Field Application

South FAE,Avnet China

深圳市宝安区新安街道创业二路与留仙一路交汇处东侧创芯研发中心1栋5楼

5th Floor, Building 1, Wise R&D Center, Liuxian 1st Road cross Chuangye 2nd Road,69th Block, Boa ’an District,Shenzhen City

O +8675586342385

M +8618026960272

D +8675586342385

F +867558378.0826

avnet.com<https://emea01.safelinks.protection.outlook.com/?url=http%3A%2F%2Favnet.com%2F&data=02%7C01%7Cws.wong%40nxp.com%7Cb1694567060e40ace47208d59de6bc7d%7C686ea1d3bc2b4c6fa92cd99c5c301635%7C0%7C0%7C636588536688437382&sdata=%2ByRoHs0%2FqgD%2BDwbxAes4iThAy8ghHMQ1AaWisaRqYqs%3D&reserved=0>

发件人: Radhika Somaiya <admin@community.nxp.com>

发送时间: 2020年5月12日 0:09

收件人: Deng, Ray <Ray.Deng@AVNET.COM>

主题: You have been mentioned by Radhika Somaiya in Re: i.MX6ULL Compile Error in NXP Community

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

You have been mentioned

by Radhika Somaiya<https://community.nxp.com/people/radhika.somaiya@volansystech.com?et=notification.mention> in Re: i.MX6ULL Compile Error in NXP Community - View Radhika Somaiya's reference to you<https://community.nxp.com/message/1310130?commentID=1310130&et=notification.mention#comment-1310130>

0 件の賞賛