i.MX6S SDMA mem_2_ssiapp script transfer no data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6S SDMA mem_2_ssiapp script transfer no data

489件の閲覧回数
torus1000
Contributor V

Hi all,

I modified i.MX6 platformSDK sample code to playback with I2S audio codec.

        sdma\test\spi_lpb.c   ecspi_app_test()
        sdma\test\uart_loopback.c   uart_app_test()

In case of NOT using SDMA, there was no problem to play.
But in case of using SDMA, nothing played(no sound).
It seems SSI asserted DMA request signal and SDMA took exact time to suit data size.

Can anybody help me...?

(Q1) Is there any tips or special settings to use SDMA/mem_2_ssiapp?

(Q2) I set destination address as "SSI Transmit Data Register : SSIn_STXn". Is it correct?

Thanks.

ラベル(1)
0 件の賞賛
1 返信

368件の閲覧回数
dauphinalexandr
Contributor II

hi,

i'm facing the same problem.

did you found a solution for this issue ?

Tks

0 件の賞賛