i.MX6QP - DDR3 vs LPDDR2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6QP - DDR3 vs LPDDR2

ソリューションへジャンプ
1,480件の閲覧回数
andrzejdziedzic
Contributor IV

Hi all

Do you know what will be the difference in perfomance between DRR3 and LPDDR2 for iMX6 QuadPlus?

Or maybe do you know about some Android device with iMX6QP and LPDDR2 which can be used for tests and compared to SABRE AI?

Best regards,

Andy

ラベル(1)
0 件の賞賛
返信
1 解決策
637件の閲覧回数
art
NXP Employee
NXP Employee

Q. Do you know what will be the difference in perfomance between DRR3 and LPDDR2 for iMX6 QuadPlus?

A. Typically, for i.MX6 series processors, the data throughput performance of the DDR3 and LPDDR2 memories is similar when operating on the same type of processor with equal data bus width and bus frequency.

Q. Or maybe do you know about some Android device with iMX6QP and LPDDR2 which can be used for tests and compared to SABRE AI?

A. No, there is no ready to use i.MX6QP + LPDDR2 device available yet.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
637件の閲覧回数
andrzejdziedzic
Contributor IV

Thanks for reply!

Best regards,

Andy

0 件の賞賛
返信
638件の閲覧回数
art
NXP Employee
NXP Employee

Q. Do you know what will be the difference in perfomance between DRR3 and LPDDR2 for iMX6 QuadPlus?

A. Typically, for i.MX6 series processors, the data throughput performance of the DDR3 and LPDDR2 memories is similar when operating on the same type of processor with equal data bus width and bus frequency.

Q. Or maybe do you know about some Android device with iMX6QP and LPDDR2 which can be used for tests and compared to SABRE AI?

A. No, there is no ready to use i.MX6QP + LPDDR2 device available yet.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信