Hi, I have a flexcan TX (output) signal doesn't working. I check with multimeter it's connected to the right micro ball but it's programmed as input... with a light 1kohm to gnd the signal fall low as an input pin. At the same time the flexcan RX (input) it seems working good. I can't understand how this is possible. Are there any driver updated or SW tool test for check this item? I'm working on i.MX6 Quad and Dual. Tks, rgds, Davide
Hi davide
one can check dts configuration flexcan example in
linux/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi
linux-imx.git - i.MX Linux Kernel
and test with Demo Images
https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_MX6QDLSOLO&appType=license&location=null
use test procedure in imx-test (../test/can)
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------