i.MX6Q5E can't send DNS in android 5.1.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q5E can't send DNS in android 5.1.1

502 Views
jimmyli
Contributor IV

Hi,

     In i.MX6Q5E platform, we run android 5.1.1 or android 6.0.1, and found that the DNS package couldn't be sent.

     Test process:

      1. DNS configuration :

          a. DNS with system setting;

          b. DNS with manual package;

     2. DNS package catching

         a. in system catching

         b. IP package catching outside

     3. Test result

         a. android 4.2.2   --OK, can catch the IP package outside

         b. android 5.1.1/6.0.1  --In system catching is OK, while IP package catching outside is not.

     Question:

     a. What cause the problem?

     b. How can we solve the problem?

     Thanks.

Labels (2)
0 Kudos
1 Reply

418 Views
diegoadrian
NXP Employee
NXP Employee

Hello Jimmy,

I apologize for the delay.

Do you know if there is a connection between your i.MX device and the modem that you are using?

The modem is recognizing the board?

Best Regards,

Diego

0 Kudos