i,MX6 DL boot from eMMC 4.51 and 5.1 difference

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i,MX6 DL boot from eMMC 4.51 and 5.1 difference

1,135 Views
qinzhengtian
Contributor I

we have a system board which includes;

i.MX6 DL

DDR3  2PCS 4Gb

4 GB eMMC 4.51(MTFC4GLWDM-4M AAT Z) connectd to USDHC3 configured for 8 bit DDR or SDR

We can flash the eMMC with u-boot using MFG tool

We can run u-boot from MFG tool

We are trying to run u-boot form User partition.

The system can work well and NO find boot issue.

But recently we changed emmc (MTFC4GACAJCN-4M IT), MMC 5.1.

Now There are some boards can't boot from emmc, if change to old chip(MTFC4GLWDM-4M AAT Z), the system work well again.  Some boards can't boot from emmc sometimes, but no body know when can't boot again. But write  emmc  always is ok.

So, we have some questions:

1. can the i.MX6  boot from eMMC 5.0 and above? 

2. If we must boot from eMMC 5.0, how did we do it? what is the eMMC configuration? are there any other needed tasks to be done?

3. if booting is not possible, any suggestion? should we add a NOR flash for u-boot? should we go down to eMMC4.4? will eMMC 4.4 going to be discontinued soon? 

Thanks for any help you can provide.

Labels (1)
0 Kudos
1 Reply

1,025 Views
igorpadykov
NXP Employee
NXP Employee

Hi jesse

in general i.MX6  can boot from eMMC 5.0 and above.

One can look at solutions provided on

eMMC 8GB to 4GB - crash on linux (yocto) boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos