i.MX28 EMI_DDR_OPEN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,308件の閲覧回数
chris321
Contributor IV

Hello Community,

I've a question for routing the EMI_DDR_OPEN trace. If I read this right the appnote AN4215 says DDR_OPEN route length equals CLK routed length + DQS routet length. But there are 2 CLK traces (CLK and CLKn) and 4 DQS (DQS0, DQS0n, DQS1, DQS1n).

Do that mean I have to sum up the matched length of DQS and the matched length of CLK?

For Example_

DQM0 = 17,1 mm

DQM0n = 17,2 mm

DQM1 = 16,9 mm

DQM1n = 16,8 mm

CLK = 11,9mm

CLK = 12,1mm

Is now the length of EMI_DDR_OPEN (17+12)mm ?

thank You

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
934件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Yes, you are right.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
934件の閲覧回数
chris321
Contributor IV

Thank you jimmychan,

I asked this question because I wondered that this formula doesn't work in the i.mx28 Design Files.

On this board I've measured:

CLK 12,3mm,

DQS0 17,4mm and

DQS1 17,1mm

with an EMI_DDR_OPEN = 35,6mm

0 件の賞賛
返信
935件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Yes, you are right.

0 件の賞賛
返信