i.MX UART hardware misbehaves on baudrate mismatch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX UART hardware misbehaves on baudrate mismatch

Jump to solution
7,412 Views
george
Senior Contributor II

Dear all,

Now, we have a issue in the product using i.MX6SX.

I searched it in this community, and I found any same issues as follows:

i.MX6 infinite loop in uart driver(rx interrupt) 

i.MX6 UART hardware misbehaves on baudrate mismatch 

It is an issue to continue receiving 0xFF as well as these reports, although there is no data reception.

As shown in the following figure, general UART communication has Start bit and Stop bit.

pastedImage_3.png

When receiving continuous data, can't the UART block for i.MX detect Start-bit and Stop-bit?

Best Regards,

George

0 Kudos
1 Solution
5,970 Views
fabio_estevam
NXP Employee
NXP Employee

Hi George,

I found a workaround for this issue.

Here is the change I made:

http://code.bulix.org/eaioxl-320184 

besides this change you also need to pass fsl,automatic-baudrate in the uart2 node:

&uart2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_uart2>;
fsl,automatic-baudrate;
status = "okay";
};

This change enables automatic baud rate detection and avoids the storm of 0xFF.

Regards,

Fabio Estevam

View solution in original post

24 Replies
2,349 Views
george
Senior Contributor II

Hi FabioEstevam‌,

Yes, two virtual COM ports are connected to my Linux PC with the USB cable.

Best Regards,

George

0 Kudos
197 Views
Yuri
NXP Employee
NXP Employee

Hello,

  It is mentioned in https://community.nxp.com/thread/441193 , that this is 

(hardware) feature of the i.MX UART module (if short start bit appears because
of noisy environment). 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
197 Views
george
Senior Contributor II

Dear Yuri‌,

That is, does it mean that the product using i.MX series has the "0xFF infinite reception" risk?

When we do not wish to do so, please tell me how to prevent it.

BR,

George

0 Kudos
197 Views
Yuri
NXP Employee
NXP Employee

Hello,

  it is needed to avoid situations, when short (non-proper) start bit appears.

In particular, it may occur if disconnecting cable during transfer.   

Regards,

Yuri.

0 Kudos