i.MX 6 - which pins are boundary scan compatible?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6 - which pins are boundary scan compatible?

1,031 Views
noobieit
Contributor I

hello, i need just a little help...

i'm trying to understand which pins of i.MX 6 are Boundary Scan compatible...

i downloaded BSDL files and i'm trying to learn how to read them...

in port description are all pins available, right? boundary and not boundary (in, out and inout are Boundary (or could be boundary???), linkage not boundary)

in the last part of BSDL i have the attribute BOUNDARY_REGISTER...what is? how could i understand it?

for ex:

-- num cell   port/*          function      safe  [ccell  dis  rslt]

"   0  (BC_4, PCIE_RXM,       observe_only, X)                       ," &

"   1  (BC_4, PCIE_RXP,       observe_only, X)                       ," &

"   2  (AC_1, PCIE_TXP,       output3,      X,    3,      0,   Z)    ," &

"   3  (BC_1, *,              control,      0)                       ," &

"   4  (BC_8, PMIC_STBY_REQ,  bidir,        X,    5,      1,   Z)    ," &

"   5  (BC_2, *,              control,      1)                       ," &

"   6  (BC_8, BOOT_MODE1,     bidir,        X,    7,      1,   Z)    ," &

Thanks to all :smileyhappy: please try to reply in an easy-english :smileyhappy:

Labels (5)
0 Kudos
Reply
1 Reply

822 Views
igorpadykov
NXP Employee
NXP Employee

Hi gigi

please look at IMX6DQ6SDLHDG  Chapter 11

Using BSDL for Board-level Testing, it explains bsdl usage.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply