i had compiled opencv 2.4.5 successfully,but it run failured as following:
root@myzr /opt/opencvtest$ ./hog pic1.png
Controls:
ESC - exit
m - change mode GPU <-> CPU
g - convert image to gray or not
1/q - increase/decrease HOG scale
2/w - increase/decrease levels count
3/e - increase/decrease HOG group threshold
4/r - increase/decrease hit threshold
Scale: 1.05
Group threshold: 8
Levels number: 13
Win width: 48
Win stride: (8, 8)
Hit threshold: 1.4
Gamma correction: 1
OpenCV Error: Gpu API call (CL_INVALID_DEVICE_TYPE) in getDevice, file /mnt/share/opencv-2.4.5/modules/ocl/src/initialization.cpp, line 312
error: /mnt/share/opencv-2.4.5/modules/ocl/src/initialization.cpp:312: error: (-217) CL_INVALID_DEVICE_TYPE in function getDevice
Segmentation fault
ocl/src/initialization.cpp lines 313 is:
309: cl_uint numsdev;
310: cl_int status = clGetDeviceIDs(platforms[i], devicetype, 0, NULL, &numsdev);
311: if(status != CL_DEVICE_NOT_FOUND)
312: openCLVerifyCall(status);
it means that the initialization is failure,so i searched in internet,and find and document <<Fast Image Processing with i.MX 6 Series>>(http://cache.freescale.com/files/32bit/doc/app_note/AN4629.pdf ) and a link (Freescale OpenEmbedded/Yocto Layers discussion list () ,but the new problem is:
(1)the pdf document Implemented the face detector,Object detection,Image processing ,but where can i download the code?
(2) the link tell that :
"You are right, the OCL module in OpenCV is CUDA based, it doesn´t work for us. Using OpenCL in this case, you can base on OpenCL embedded profile tutorials you can find in the web also, I created a simple OCL SDK, that provides you a quick start for opencl application, unfortunately it is not available outside Freescale yet, there are some samples there (IP filtering) that you could use, I just need to check if I can share right now",
who can tell me: is it right that "the OCL module in OpenCV is CUDA based, it doesn´t work for imx6"? the author created a simple OCL SDK ,but where is it,can i use it?
can you answer me as soon as possible? it is hurry!!
hello,I want to know that do you use the ocl in opencv with imx6q successfully?
what is your solution? thanks。
Hi Xuelong,
OCL in OCV is not supported on imx6q (embedded profile), only on imx6qp.
cheers,
andre
Hello,I am a graduate student, I download your code about opencl from GitHub - andreluizeng/opencl: i.MX OpenCL + OpenCV sample codes。I make it success,but when I run ./cl_helloworld on my board(imx6q, Linux 3.0.35),There are some questions: sometimes it run success;sometimes it run error,the one kind of error messages as following:
Initializing OpenCL: Ok
-=-=-=- Platform Information -=-=-=-
Platform Name: Vivante OpenCL Platform
Platform Profile: EMBEDDED_PROFILE
Platform Version: OpenCL 1.1
Platform Vendor: Vivante Corporation
-=-=-=- Device Information -=-=-=-
Device Name: Vivante OpenCL Device
Device Profile: EMBEDDED_PROFILE
Device Version: OpenCL 1.1
Device Vendor: Vivante Corporation
Device Max Work Item Dimensions: 3-D
Device Max Work Group Size: 1024
-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-
Loading CL programs: hello_world Ok
Building hello_world kernel:
*** glibc detected *** ./cl_helloworld: malloc(): memory corruption: 0x00022768 ***
Aborted
another kind of error messages as following:
Initializing OpenCL: Ok
-=-=-=- Platform Information -=-=-=-
Platform Name: Vivante OpenCL Platform
Platform Profile: EMBEDDED_PROFILE
Platform Version: OpenCL 1.1
Platform Vendor: Vivante Corporation
-=-=-=- Device Information -=-=-=-
Device Name: Vivante OpenCL Device
Device Profile: EMBEDDED_PROFILE
Device Version: OpenCL 1.1
Device Vendor: Vivante Corporation
Device Max Work Item Dimensions: 3-D
Device Max Work Group Size: 1024
-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-
Loading CL programs: hello_world Ok
Building hello_world kernel:
cl_helloworld: malloc.c:3096: sYSMALLOc: Assertion `(old_top == (((mbinptr) (((char *) &((av)->bins[((1) - 1) * 2])) - __builtin_offsetof (struct malloc_chunk, fd)))) && old_size == 0) || ((unsigned long) (old_size) >= (unsigned long)((((__builtin_offsetof (struct malloc_chunk, fd_nextsize))+((2 * (sizeof(size_t))) - 1)) & ~((2 * (sizeof(size_t))) - 1))) && ((old_top)->size & 0x1) && ((unsigned long)old_end & pagemask) == 0)' failed.
Aborted
I think the program stopped at Line 610(cl_helloworld.cpp) “ error = clBuildProgram ((* program), 1, device_id, "", NULL, NULL);”,but I cannot solve it. I hope I can get your help. Thank you!
Are you using a NXP or a custom board ? I have been working a much newer kernel and GPU driver (which is the recomendation) is it possible to do some tests a 4.1.15 kernel ?
regards,
Andre
Please refer to attached document for the detailed information on the graphics features, supported by the i.MX6 platform.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I downloaded this file and simply looked at it, and didn't find what I needed.
I need the sourcecode of object detection and face recognition or gesture recognition demo in the <<Fast Image Processing with i.MX 6 Series>> ,or the OCL sdk which can replace the ocl module in opencv.
thanks.
There is no source code available. The AN4629 just describes the basic principles, all other work is up to you.
Artur
oh, the screenshots in AN4629 are artificial?