esai 调试数据引脚ESAI_TX2_RX3 无波形输出

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

esai 调试数据引脚ESAI_TX2_RX3 无波形输出

1,747 Views
2570624484
Contributor II

Deal NXP :

软件环境 :Android7.1.1  BSP :kernel 4.10.0

硬件IMX6Q,不使用asrc,只需要esai接口

您好:正在调试IMX6q 的esai audio的放音,现在只用到三个引脚,如下dts配置(已经查了好几遍,没有其他驱动复用这三个引脚),bitclk 和lrclk(44.1K)在用tinyplay播放音乐的时候都有正确的时钟输出,但数据引脚TX2_RX3没有波形变化,在dma完成函数里加打印,也可以看到打印在播放的时候不停地输出。

dts如下:

 dspsi47920_codec: dspsi47920_codec {
                #sound-dai-cells = <0>;
                compatible = "dspsi47920-codec-play";
        };
  sound-si47920-esai {
   compatible ="fsl,imx-audio-si47920";
    model = "imx-si47920";
    esai-controller = <&esai>;   
   // asrc-controller = <&asrc>;//not uesd asrc
    audio-codec = <&dspsi47920_codec>;
  };   

&esai {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_esai>;
 assigned-clocks = <&clks IMX6QDL_CLK_ESAI_SEL>,
     <&clks IMX6QDL_CLK_ESAI_EXTAL>;
 assigned-clock-parents = <&clks IMX6QDL_CLK_PLL4_AUDIO_DIV>;
 assigned-clock-rates = <722534400>, <22579200>;
 
 status = "okay";
 fsl,esai-synchronous;
};

  pinctrl_esai: esaigrp {
   fsl,pins = <
    MX6QDL_PAD_ENET_CRS_DV__ESAI_TX_CLK 0x1b030
    MX6QDL_PAD_ENET_RXD1__ESAI_TX_FS    0x1b030
    MX6QDL_PAD_ENET_TXD1__ESAI_TX2_RX3  0x1b030
    
   >;
  };

期待你的尽快回答,已经搁置还几天。非常感谢。

0 Kudos
3 Replies

1,283 Views
jimmychan
NXP TechSupport
NXP TechSupport

Attached is the Linux Reference manual. Please read the Chapter 7 for the Audio driver. Our driver is needed to use asrc.

0 Kudos

1,283 Views
2570624484
Contributor II

HI  jimmychan

   不需要asrc是可以的,如果默认是从TX0输出的话,esai 的代码是不需要修改的,由于我们的硬件是从ESAI_TX2输出,esai的驱动代码是需要稍微改动一下。

0 Kudos

1,283 Views
2570624484
Contributor II

Dear NXP:

         我这里实在没有找到原因。

我做了个实验,将MX6QDL_PAD_ENET_TXD1配置为普通的人GPIO功能 MX6QDL_PAD_ENET_TXD1__GPIO1_IO29

做如下的控制:

echo 29 > /sys/class/gpio/export 
echo "out" >  /sys/class/gpio/gpio29/direction 
echo 1 >   /sys/class/gpio/gpio29/value
echo 0 >   /sys/class/gpio/gpio29/value

测量GPIO的引脚变化高低正常。

还请NXP同事辛苦分析一下,为何MX6QDL_PAD_ENET_TXD1__ESAI_TX2_RX3功能不正常。非常感谢!!!

0 Kudos