embed camera to i.MX53 quick start board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

embed camera to i.MX53 quick start board

Jump to solution
2,223 Views
alexanderkozlov
Contributor II

Hi,

I've recieved i.MX53 QSB and I would like to embed OmniVision sensor to it. As I understand an expansion header supports CSI camera to be connected and there is a standart board-to-board connector for expansion header. But I don't know about camera boards that supports such connector.

So, is there any camera boards with OmniVision or other image sensors for i.MX53 QSB? If not, what I need to do to embed camera to QSB?

Thanks in advance for any answer,

Alexander

Labels (1)
0 Kudos
1 Solution
1,392 Views
alexanderkozlov
Contributor II

Thanks!

Will try like scheme below:

OV7620's pins - Exp. header's pins

1 - 59

2 - 24

3 - 29

4 - 3

5 - 31

6 - 33

7 - 58

8 - 53

9 - 56

10 - 17

11 - 19

12 - 52

13 - 38

14 - 50

15 - 30

16 - 46

17 - 35

18 - 44

19 - 26

20 - 34

21 - 28

22 - 32

23 - 21 (No connect)

24 - 22 (No Connect)

But I am not sure about 1st and 6th sensor's pins.

In OV7670 datasheet says the following:

Pin    Number Name    Pin Type      Function/Description

01     STRB                Output          LED/strobe control output

06     RESET             # Function     Chip reset, active low

                                (default = 1)

May be 6th pin should be maped to 59 IMX pin (CSI_RSTB) that is RESET pin as I undestand. But what to do with 1st sensor's pin in this case?

View solution in original post

0 Kudos
11 Replies
1,392 Views
jimmychan
NXP TechSupport
NXP TechSupport

Please download the QSB schematic from the i.MX53QSB web page. In the page 13, there is a connector J13. The CSI0 signals are linked to this J13. You can make your adapter board with your camera and then connect it to this J13.

0 Kudos
1,392 Views
alexanderkozlov
Contributor II

Thanks a lot! But what document do you mean?

May be http://cache.freescale.com/files/32bit/doc/user_guide/IMX53QSBRM.pdf?fpsp= ?

0 Kudos
1,392 Views
jimmychan
NXP TechSupport
NXP TechSupport
0 Kudos
1,392 Views
alexanderkozlov
Contributor II

Thanks. This scheme is the same as in the document that mentionted by me.

I have OmniVision sensor OV7670 with 24 pins described here http://i01.i.aliimg.com/img/pb/912/479/406/406479912_434.jpg. As I see it has 10 data pins that are D0 - D9. And I don't undestand how to map them to exp. header because I found only 8 data pins on scheme: CSI0_DAT12 - CSI0_DAT19.

0 Kudos
1,392 Views
jimmychan
NXP TechSupport
NXP TechSupport

As the exp. header only have CSI0_DAT12 - CSI0_DAT19, this only can support 8-bit mode. So please check the OV7670 datasheet. It should able to set to work in 10bit mode and 8bit mode. And the datasheet should show you which data pins are for 8bit.

0 Kudos
1,393 Views
alexanderkozlov
Contributor II

Thanks!

Will try like scheme below:

OV7620's pins - Exp. header's pins

1 - 59

2 - 24

3 - 29

4 - 3

5 - 31

6 - 33

7 - 58

8 - 53

9 - 56

10 - 17

11 - 19

12 - 52

13 - 38

14 - 50

15 - 30

16 - 46

17 - 35

18 - 44

19 - 26

20 - 34

21 - 28

22 - 32

23 - 21 (No connect)

24 - 22 (No Connect)

But I am not sure about 1st and 6th sensor's pins.

In OV7670 datasheet says the following:

Pin    Number Name    Pin Type      Function/Description

01     STRB                Output          LED/strobe control output

06     RESET             # Function     Chip reset, active low

                                (default = 1)

May be 6th pin should be maped to 59 IMX pin (CSI_RSTB) that is RESET pin as I undestand. But what to do with 1st sensor's pin in this case?

0 Kudos
1,392 Views
jimmychan
NXP TechSupport
NXP TechSupport

Is it a typo in your scheme? your scheme show pin 6 is to 33. the correct one should be 59?

For the STRB pin, I think the usage is depends on your application.

e.g. it can be used for triggering a flash. In the below AN, the Figure 10 is an example.

< http://www.skyworksinc.com/uploads/documents/AATI_AN_61.pdf >

1,392 Views
alexanderkozlov
Contributor II

It was my first opinion that pin 6 should be connected to pin 33. But it's not true and now I'm pretty sure that pin 6 is mapped to pin 59 on QSB.

I also suppose to keep pin 1 unconnected because I have no LED/Flash.

So, new scheme are here:

1 - 23 (No connect)

2 - 24

3 - 29

4 - 3

5 - 31

6 - 59

7 - 58

8 - 53

9 - 56

10 - 17

11 - 19

12 - 52

13 - 38

14 - 50

15 - 30

16 - 46

17 - 35

18 - 44

19 - 26

20 - 34

21 - 28

22 - 32

23 - 21 (No connect)

24 - 22 (No Connect)

0 Kudos
1,392 Views
BrilliantovKiri
Senior Contributor I

Hello, Alexander!

You can make simple adapter.

0 Kudos
1,392 Views
alexanderkozlov
Contributor II

Thank Kirill,

But I am not good at hardware. Could you please provide any reference or an example of such adapter?

0 Kudos
1,392 Views
BrilliantovKiri
Senior Contributor I

Hello, Alexander!

Sorry, I also only programmer.

0 Kudos