drivers for serializer(DS90UB927Q-Q1)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

drivers for serializer(DS90UB927Q-Q1)

801 Views
rambabugedela
Contributor I

hi,

I am working on serializer (DS90UB927Q-Q1) for sabresd board (IMX6dl) but I found that there no drivers for DS90UB927Q-Q1. Anybody help me plz.

Labels (4)
0 Kudos
Reply
1 Reply

514 Views
art
NXP Employee
NXP Employee

Do you use the i.MX6 series Linux BSP by NXP? If so, to perform the serializer IC configuration through the I2C control interface, you can use the low-level I2C driver, already included into the system. For more details, refer to the Chapter 37 of the attached document. In all other aspects, no other special driver is required for the DS90UB927Q serializer IC operation.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply