display issues with 3.14 kernel on imx53 boards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

display issues with 3.14 kernel on imx53 boards

2,200件の閲覧回数
belgianwaffle
Contributor II

We are having some issues with the display settings in the device tree not being set. I am seeing the same issue on our imx53 based board and on the imx53-qsb eval board (formally LOCO).

Basically when I check settings with fbset, they are not what's in the dts.

For example here is the eval board dts...

display@di0 {

    compatible = "fsl,imx-parallel-display";

    crtcs = <&ipu 0>;

    interface-pix-fmt = "rgb565";

    pinctrl-names = "default";

    pinctrl-0 = <&pinctrl_ipu_disp0_1>;

    status = "disabled";

    display-timings {

        claawvga {

            native-mode;

            clock-frequency = <27000000>;

            hactive = <800>;

            vactive = <480>;

            hback-porch = <40>;

            hfront-porch = <60>;

            vback-porch = <10>;

            vfront-porch = <10>;

            hsync-len = <20>;

            vsync-len = <10>;

            hsync-active = <0>;

            vsync-active = <0>;

            de-active = <1>;

            pixelclk-active = <0>;

        };

    };

};

And here is fbset output...

root@freescale ~$ fbset

mode "1024x768"

    geometry 1024 768 1024 768 16

    timings 0 0 0 0 0 0 0

    accel true

    rgba 5/11,6/5,5/0,0/0

endmode

As you can see the setting are not correct and the timings are all zero's.

Here's the relevant sys.log excerpt...

imx-drm imx-drm: No connectors reported connected with modes

[drm] Cannot find any crtc or sizes - going 1024x768

Console: switching to colour frame buffer device 128x48

imx-drm imx-drm: fb0:  frame buffer device

imx-drm imx-drm: registered panic notifier

Our custom board behaves about the same way with similar sys.log messages.

The eval board display has a bunch of lines. Our board seems a bit better with just the colors being off. Presumably because the timings are all zero's. I'm also seeing the same issue on our mx51 based system.

I was really hoping the eval board was going to work with the latest kernel since we are in the middle of upgrading also.  Am I missing something? Any help would be greatly appreciated as to why the dts display settings are not being set.

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,305件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Comparing with this example I found:

disp1: display@disp1 {

       compatible = "fsl,imx-parallel-display";

       pinctrl-names = "default";

       pinctrl-0 = <&pinctrl_disp1_1>;

       crtcs = <&ipu 1>;

       interface-pix-fmt = "rgb24";

      status = "okay";

      display-timings {

            tx14d11vm1cpd {

            clock-frequency = <5847953>;

            hactive = <320>;

            vactive = <240>;

            hfront-porch = <30>;

            hback-porch = <30>;

            hsync-len = <5>;

            vback-porch = <5>;

            vfront-porch = <6>;

            vsync-len = <2>;

            pixelclk-active = <1>;

            hsync-active = <0>;

            vsync-active = <0>;

            de-active = <1>;

            };

       };

  };

I noticed that you are not enabling the device. The status is disabled.

Can you try changing that property?

/Alejandro

0 件の賞賛
返信

1,305件の閲覧回数
belgianwaffle
Contributor II

Hi Alejandro,

I set the status to ok after I posted my initial question, but it did not solve the issue.

What solved the color issue in our case was to set interface-pix-fmt = "bgr666".

fbset still reports all zero's for timings though, even though they are ok internally. Looks like the DRM doesn't report it.

0 件の賞賛
返信

1,305件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I found this discussion in linux-arm-kernel

http://lists.infradead.org/pipermail/linux-arm-kernel/2013-June/180781.html

DRM doesn't provide full information via fbdev - its fbdev is just a

compatibility later nothing more.

/Alejandro

0 件の賞賛
返信