Hello,
We start to use imxRT 1050, MCUExpresso, freeRTOS, with a memory unit for boot , not sure yet exactly which hyperFlash, qspi, or spi nor flash, (it shall be decided according to the answers), but it is required that the application shall copy itself to RAM and starts running from RAM.
I read carefully AN12107, "How to Enable Boot from Octal SPI Flash and SD Card", yet still not sure:
I see that linked file <name>.icf contains:
But it is not explained what the meaning of each of this values:
Thank you,
ranran
解決済! 解決策の投稿を見る。
Hi ranran
data_start/end,data2_start/end are described in icf files (like MIMXRT1052xxxxx_sdram.icf )
included in
Users Guide (4)
i.MXRT1050 EVK Extended Feature Example Code and HW guide
i.MX RT1050 MCU/Applications Crossover Processor | Arm® Cortex®-M7 @600 MHz, 512KB SRAM |NXP
I do not think that "m_start_text in icf = startaddress +ivtOffset +initialLoadSize", as it can be in any place
above startaddress +ivtOffset.
Best regards
igor
Hi ranran
for ram example one can look on
RT1050 - Booting from serial NOR flash to SDRAM
>Why example for "3.6. MFG boot from Hyper Flash with DCD for SDRAM" uses
>offset 0x400 (which is used for non-xip) ?
please check Figure 8-14. Image Vector Table i.MX RT1050 Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf
So if "Dest.Memory" is the same as "Boot Device Memory", then it is xip, if different - then non-xip.
For IAR linked file <name>.icf structure description one can look at IAR documentation
http://supp.iar.com/FilesPublic/UPDINFO/011453/arm/doc/EWARM_DevelopmentGuide.ENU.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
>So if "Dest.Memory" is the same as "Boot Device Memory", then it is xip, if different - then non-xip.
But in the given example
RT1050 - Booting from serial NOR flash to SDRAM
File imx-sdram-normal-unsigned-dcd.bd contains "ivtOffset = 0x1000;"
As I understand 0x1000 means it is xip , so "Dest.Memory" should be the same as "Boot Device Memory".
But it is not the same : boot from serialNOR to SDRAM.
How can it be ?
Best Regards,
ranran
you should look for "boot_data" (absolute address where rom copies image)
sect.8.7.1.2 Boot data structure Reference Manual.
0x1000 means that this is "offset" described in Table 8-36. Image Vector Table Offset and Initial Load Region Size.
Best regards
igor
Hello Igor,
Thank you very much for the information.
It seems, as far as I understand, that there is a mistake in AN12107.pdf :
In section 3.6 , .bd file in page 40 shows:
startaddress = 0x60000000
ivtOffset = 0x1000
initialLoadSize = 0x2000
--> I expects that m_start_text in icf = startaddress +ivtOffset +initialLoadSize = 0x60003000 , but
the icf file shows (step 3, page 37):
m_start_text = 0x60002400
Note that a similar example with icf file and bd file in section 3.5 shows icf file with m_start_text value exactly as expected from the given .bd file in that section (I am using the same calculation : m_start_text in icf = startaddress +ivtOffset +initialLoadSize).
Is it correct that there is a mistake with m_start_text value in .icf given in page 37 ?
Thank you very much for the time,
ranran
Hi ranran
data_start/end,data2_start/end are described in icf files (like MIMXRT1052xxxxx_sdram.icf )
included in
Users Guide (4)
i.MXRT1050 EVK Extended Feature Example Code and HW guide
i.MX RT1050 MCU/Applications Crossover Processor | Arm® Cortex®-M7 @600 MHz, 512KB SRAM |NXP
I do not think that "m_start_text in icf = startaddress +ivtOffset +initialLoadSize", as it can be in any place
above startaddress +ivtOffset.
Best regards
igor
Hello Igor,
Where can I read how to set the values in bd file ? (startaddress ,ivtOffset ,initialLoadSize, etc) It's not described in elftosb user guide.
Thank you,
ranran