clock signal through gpios in imx6 dual lite

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

clock signal through gpios in imx6 dual lite

1,585 次查看
sribinkr
Contributor I

hi,

      I want to give configurable cpu clock through a gpio.Someone pls explain me the steps involved in setting the frequency and giving out through gpio in imx6 dual lite cpu in linux environment.I have the yocto source code downloaded for the iwave custom board using imx6 dl cpu.

标记 (1)
0 项奖励
回复
3 回复数

861 次查看
art
NXP Employee
NXP Employee

Do you mean the CCM_CLKO1 and CCM_CLKO2 clock output signals? If so, you first have to select the desired pad for the signal by appropriately configuring the IOMUX module, refer to the Sections 3.5 and 3.6 of attached Linux Reference Manual document. Then, unfortunately, there are no regular tools to control the CCM_CLKx source to output in the user space. The only way to control it is to directly access the CCM_CCOSR register by a physical address through /dev/mem.

Also, please refer to attached Linux BSP Porting Guide document for various aspects of customizing the Linux BSP.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

861 次查看
sribinkr
Contributor I

Thanks..how to configure ccm _clk01 from linux user space?

0 项奖励
回复

861 次查看
joanxie
NXP TechSupport
NXP TechSupport

for how to change the cpu frequency, pls refer to the chapter 18 of enclosed file.

0 项奖励
回复