about ADC sampling clock-2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about ADC sampling clock-2

Jump to solution
730 Views
goto11
Contributor III

hello,

 

Table 93. Recommended operating conditions for 12-bit ADC in .MX 7 Dual Family of Applications Processors Datasheet
Is it OK to make the RIEXT value larger than 250Ω (for example, from several kΩ to dozens of kΩ) when FCLK and FSOC are operated at close Min values?

What kind of problems will occur if the resistance value is increased?

 

best regards

Goto

Labels (1)
0 Kudos
Reply
1 Solution
635 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

>Is it OK to make the RIEXT value larger than 250Ω..

not, sorry.

>What kind of problems will occur if the resistance value is increased?

it may affect measurement accuracy, details can be found on web, for example :

Required output impedance for ADC input? - Electrical Engineering Stack Exchange 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
636 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

>Is it OK to make the RIEXT value larger than 250Ω..

not, sorry.

>What kind of problems will occur if the resistance value is increased?

it may affect measurement accuracy, details can be found on web, for example :

Required output impedance for ADC input? - Electrical Engineering Stack Exchange 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply