Wifi not enabling on EDM1-IMX6P REV: B1  Android 8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wifi not enabling on EDM1-IMX6P REV: B1  Android 8

846 Views
aniket_m
Contributor I

Hi,
I am trying to enable my wifi on my EDM1-IMX6P REV: B1  Android 8 both manually as well as programatically. But its giving me below error

2021-08-20 22:19:30.695 274-274/? I/android.hardware.wifi@1.0-service: Wifi HAL started
2021-08-20 22:19:30.701 274-274/? E/android.hardware.wifi@1.0-service: Could not read interface state for wlan0 (No such device)
2021-08-20 22:19:30.702 274-274/? E/android.hardware.wifi@1.0-service: Failed to set WiFi interface up
2021-08-20 22:19:30.702 274-274/? E/android.hardware.wifi@1.0-service: Failed to start legacy HAL: UNKNOWN
2021-08-20 22:19:30.702 410-499/system_process E/HalDeviceManager: executeChipReconfiguration: configureChip error: 9 (unknown)
2021-08-20 22:19:30.909 274-274/? I/android.hardware.wifi@1.0-service: Wifi HAL stopped
2021-08-20 22:19:30.909 274-274/? E/hw-IPCThreadState: binder thread pool (1 threads) starved for 206 ms
2021-08-20 22:19:30.910 410-499/system_process E/WifiNative-wlan0: Failed to start HAL for client mode
2021-08-20 22:19:30.912 410-410/system_process E/WifiController: WifiControllerWifi turn on failed
2021-08-20 22:19:30.914 410-499/system_process I/WifiVendorHal: Vendor Hal stopped

The toggle button resets once pressed.

0 Kudos
3 Replies

763 Views
aniket_m
Contributor I

Hi Igor,
      I am using EDM1-IMX6Q-10-R20-E16-9377 board

0 Kudos

763 Views
aniket_m
Contributor I

Hi Igor,
               Thanks for reply i tried with below link https://wireless.wiki.kernel.org/en/users/Drivers/brcm80211
I renamed brcmfmac4330.bin tp brcmfmac-stdio.bin and added to my "vendor/nxp/imx-firmware/brcm" path and also added bcm43xx-0.fw and bcm43xx-hdr-0.fw to "vendor/nxp/imx-firmware/brcm" path but still wifi showing same error

Whereas second link https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Porting-BCM4330-BCM43362-WIFI-to-Android... is showing for Android 4 whereas i am using Android 8.

Thanks and Regards,
Aniket

0 Kudos

819 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos