Wi-Fi capability of i.Mx 8M Nano evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wi-Fi capability of i.Mx 8M Nano evk

Jump to solution
2,381 Views
dibyajyoti
Contributor II

Does the EVK come with Wi-Fi in built? Or do I need to buy a wi-fi module separately? If so, what are some of the modules that are compatible with the evk?

Labels (1)
Tags (1)
1 Solution
2,159 Views
romitchatterjee
Contributor V

You can download it from NXP: i.MX Software and Development Tools | NXP 


Select i.MX BSP Updated and Releases -> Linux -> Linux 4.14.98_2.2.0 for i.MX 8M Nano GA

View solution in original post

7 Replies
2,159 Views
dibyajyoti
Contributor II

Thanks a lot guys! By the way, I see the 8M Nano evk getting started mentions running Android. Can I run Linux on it instead?

0 Kudos
2,159 Views
romitchatterjee
Contributor V

Yes, the evk supports Linux and FreeRTOS in addition to Android.

2,159 Views
dibyajyoti
Contributor II

Great! Where can I get the Linux BSP?

0 Kudos
2,160 Views
romitchatterjee
Contributor V

You can download it from NXP: i.MX Software and Development Tools | NXP 


Select i.MX BSP Updated and Releases -> Linux -> Linux 4.14.98_2.2.0 for i.MX 8M Nano GA

2,159 Views
romitchatterjee
Contributor V

Hi felixradensky‌ - thanks for that clarification. Yes, Murata 1CX is indeed PCIe based. So I guess Murata modules 1DX (https://wireless.murata.com/type-1dx.html ) and 1LV (https://wireless.murata.com/type-1lv.html ) can also be used with i.MX 8M Nano? These two are SDIO based, similar to 1MW.

0 Kudos
2,159 Views
romitchatterjee
Contributor V

The i.MX 8M Nano EVK comes with Murata 1MW module on board (https://wireless.murata.com/type-1mw.html ). It is a very capable module with dual band (2.4 GHz, 5 GHz) 802.11 a/b/g/n/ac Wi-Fi. It also has Bluetooth 5.0.

You can also buy separate Wi-Fi modules if you want. The EVK has a M.2 connector on board, which means you can also plug in a Murata 1CX module, which provides even higher performance with dual band 802.11 a/b/g/n/ac MIMO + Bluetooth 5.0 (https://wireless.murata.com/type-1cx.html ).

0 Kudos
2,159 Views
felixradensky
Contributor IV

Hi Romit,

i.MX8M NANO has no PCIE, so connecting Murata 1CX module is not going to work.

Felix.