Why does my GICD_TYPER (ICDICTR) register indicate a higher number of CPU interfaces than cores, and could this create a problem for interrupts?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why does my GICD_TYPER (ICDICTR) register indicate a higher number of CPU interfaces than cores, and could this create a problem for interrupts?

784 Views
shefft
Contributor IV

I'm on a Solo, but bits [7:5] show 001 (two interfaces) instead of 000 (one interface).  What does that mean? i.e. what exactly is a 'CPU Interface'?  How does this register get set?

Labels (2)
0 Kudos
2 Replies

643 Views
shefft
Contributor IV

I ask because of an SGI problem I;m having with the Freescale Platform SDK and the GIC unit test.  The processor never gets to the registered interrupt service routine.  The interrupt is triggered and even acknowledged.

0 Kudos

643 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Tyler

     It is OK for this register's value being 001 even on a Solo. The CPU interface means, this is a private interface for each core, although its address is same, 0xa00100 is the GIC_CPU interface's base address, but each core will need to enable it before getting it start to work. In our v3.0.35 kernel, when booting up secondary core, arch/arm/mach-mx6/platsmp.c's platform_secondary_init will call gic_secondary_init to initialize this secondary core's GIC CPU interface.

     So, in a word, GIC_DIST is common, all cores' read/write into GIC_DIST will impact same DIST interface. But for GIC_CPU interface, each core has its own interface, can only be seen/read/write by its core.

     On your solo, as only CPU0's GIC_CPU interface is initialized, so it is OK. I think this register can NOT be set in runtime, it is a fixed  value by hardware design.

0 Kudos