Where is the u-boot code to set i.MX6DQ VDD_ARM_CAP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the u-boot code to set i.MX6DQ VDD_ARM_CAP?

Jump to solution
2,146 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ u-boot for L3.10.17_1.0.2_ga.

I'm looking for the source codes to set VDD_ARM_CAP, VDD_SOC_CAP, and VDD_PU_CAP.

Then, I found the following post and  the code is in <u-boot>/arch/arm/cpu/armv7/mx6/soc.c.

u-boot VDD_SOC_CAP, VDD_PU_CAP

According to this file, VDD_SOC_CAP is set to 1.2V and VDD_PU_CAP.

However, I could not find the code to set VDD_ARM_CAP.

Then, would you let me know where is the code to set VDD_ARM_CAP?

Best Regards,

Satoshi Shimoda

Labels (4)
Tags (3)
0 Kudos
1 Solution
1,114 Views
yurirellosa
Contributor IV

Hello Shimoda-san

On my u-boot version it has the following code:

enum ldo_reg {

  LDO_ARM,

  LDO_SOC,

  LDO_PU,

};

/*

* Set the PMU_REG_CORE register

*

* Set LDO_SOC/PU/ARM regulators to the specified millivolt level.

* Possible values are from 0.725V to 1.450V in steps of

* 0.025V (25mV).

*/

static int set_ldo_voltage(enum ldo_reg ldo, u32 mv)

{

  struct anatop_regs *anatop = (struct anatop_regs *)ANATOP_BASE_ADDR;

  u32 val, step, old, reg = readl(&anatop->reg_core);

  u8 shift;

  if (mv < 725)

  val = 0x00; /* Power gated off */

  else if (mv > 1450)

  val = 0x1F; /* Power FET switched full on. No regulation */

  else

  val = (mv - 700) / 25;

  clear_ldo_ramp();

  switch (ldo) {

  case LDO_SOC:

  shift = 18;

  break;

  case LDO_PU:

  shift = 9;

  break;

  case LDO_ARM:

  shift = 0;

  break;

  default:

  return -EINVAL;

  }

  old = (reg & (0x1F << shift)) >> shift;

  step = abs(val - old);

  if (step == 0)

  return 0;

  reg = (reg & ~(0x1F << shift)) | (val << shift);

  writel(reg, &anatop->reg_core);

  /*

  * The LDO ramp-up is based on 64 clock cycles of 24 MHz = 2.6 us per

  * step

  */

  udelay(3 * step);

  return 0;

}

int board_postclk_init(void)

{

  set_ldo_voltage(LDO_SOC, 1175); /* Set VDDSOC to 1.175V */

  return 0;

}

Maybe you could use this to set the voltage on your end.

Best regards

Yuri

View solution in original post

6 Replies
1,115 Views
yurirellosa
Contributor IV

Hello Shimoda-san

On my u-boot version it has the following code:

enum ldo_reg {

  LDO_ARM,

  LDO_SOC,

  LDO_PU,

};

/*

* Set the PMU_REG_CORE register

*

* Set LDO_SOC/PU/ARM regulators to the specified millivolt level.

* Possible values are from 0.725V to 1.450V in steps of

* 0.025V (25mV).

*/

static int set_ldo_voltage(enum ldo_reg ldo, u32 mv)

{

  struct anatop_regs *anatop = (struct anatop_regs *)ANATOP_BASE_ADDR;

  u32 val, step, old, reg = readl(&anatop->reg_core);

  u8 shift;

  if (mv < 725)

  val = 0x00; /* Power gated off */

  else if (mv > 1450)

  val = 0x1F; /* Power FET switched full on. No regulation */

  else

  val = (mv - 700) / 25;

  clear_ldo_ramp();

  switch (ldo) {

  case LDO_SOC:

  shift = 18;

  break;

  case LDO_PU:

  shift = 9;

  break;

  case LDO_ARM:

  shift = 0;

  break;

  default:

  return -EINVAL;

  }

  old = (reg & (0x1F << shift)) >> shift;

  step = abs(val - old);

  if (step == 0)

  return 0;

  reg = (reg & ~(0x1F << shift)) | (val << shift);

  writel(reg, &anatop->reg_core);

  /*

  * The LDO ramp-up is based on 64 clock cycles of 24 MHz = 2.6 us per

  * step

  */

  udelay(3 * step);

  return 0;

}

int board_postclk_init(void)

{

  set_ldo_voltage(LDO_SOC, 1175); /* Set VDDSOC to 1.175V */

  return 0;

}

Maybe you could use this to set the voltage on your end.

Best regards

Yuri

1,114 Views
satoshishimoda
Senior Contributor I

Hi Yuri,

Thank you for your reply.

Then, would you let me know where is the above code?

And the code seems to set only VDDSOC.

Is VDDARM_CAP set by iROM and not changed by u-boot?

Best Regards,

Satoshi Shimoda

0 Kudos
1,114 Views
yurirellosa
Contributor IV

Hello Shimada-san

It is the same file in my version of uboot --> /arch/arm/cpu/armv7/mx6/soc.c

My u-boot version is u-boot-fslc-2014.10.(https://github.com/Freescale/u-boot-fslc)  What version do you use?

On the example just change the code to:

set_ldo_voltage(LDO_ARM, xxxxx);  // xxxxx is the voltage you want

Best Regards.

Yuri

1,114 Views
satoshishimoda
Senior Contributor I

Hi Yuri,

Would you give me a comment whether L3.10.17_1.0.2-ga u-boot set VDD_ARM_CAP voltage?

Best Regards,

Satoshi Shimoda

0 Kudos
1,114 Views
Yuri
NXP Employee
NXP Employee

As for power supply voltage setting, mainly it is configured

(after PMIC hardware-coded initialization at power on) in U-boot.

Please refer to “board/freescale/mx6q_sabresd/mx6q_sabresd.c”

for the SDB/SDP designs.

   Further voltages also can be changed dynamically, when using DVFS.

Please look the next chapters in the Linux Reference Manual :

- "CPU Frequency Scaling (CPUFREQ) Driver"

- "Dynamic Bus Frequency Driver)"

- "PF100 Regulator Driver)"

- "Low-level Power Management (PM) Driver"

In particular, in the recent Linux BSP :

"For CPU frequency working point settings, see:

• arch/arm/boot/dts/imx6q.dtsi for i.MX 6Quad

• arch/arm/boot/dts/imx6dl.dtsi for i.MX 6DualLite

• arch/arm/boot/dts/imx6sl.dtsi for i.MX 6SoloLite

• arch/arm/boot/dts/imx6sx.dtsi for i.MX 6SoloX"

Regards,

Yuri.

0 Kudos
1,114 Views
satoshishimoda
Senior Contributor I

Hi Yuri,

I'm using L3.10.17_1.0.2-ga, so u-boot revision is 2013.04.

And in this revision, the I cannot find the above code.

I understood I can add the above code to our u-boot.

But in this post, I want to know whether VDDARM is set by u-boot for L3.10.17_1.0.2-ga (rev 2013.04).

According to your reply, VDDARM is not set by u-boot (2013.04) default code.

Is this correct?

Best Regards,

Satoshi Shimoda

0 Kudos