Where can I download libdigiapix?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I download libdigiapix?

655件の閲覧回数
liuyonggang
Contributor III
Links:ADC API | ConnectCore 8x 
Links:dey-examples/apix-adc-example at dey-2.6/maint · digi-embedded/dey-examples · GitHub 
#include <libdigiapix/adc.h>

I write a adc app test programme.I need "libdigiapix/adc.h" header.But I don't Where can download
it?

BRs
Johnny
0 件の賞賛
返信
2 返答(返信)

608件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Liu Yonggang,

The Digi ConnectCore 8X is manufactured and supported by Digi so I would recommend looking trough their documentation. Chances are this header is included as part of one of their BSPs:

https://www.digi.com/resources/documentation/digidocs/embedded/cc8x_home.html

I hope this helps!

Regards,

0 件の賞賛
返信

608件の閲覧回数
liuyonggang
Contributor III

Hi gusarambula,

    Would you please have better solution to read adc value from /dev/iio:device0 device file.I need read adc value from ADC_IN0~ADC_IN5 in app programme(except using cat /sys/bus/iio/devices/iio\:device0/in_voltage0_raw).

Tks!

BRs

0 件の賞賛
返信