When iMX6Q-SDB GPC Interrupt Controller start to work?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When iMX6Q-SDB GPC Interrupt Controller start to work?

442 Views
mileswang
Contributor II

Hello,

As we know iMX6Q-SDB GPC Interrupt Controller (INTC) is used to generate the wakeup signal. Before system enter deep sleep mode (DSM), can it generate intereupt (a bit of GPC_ISRx is set)? I met a problem about wakeup.

In normal case, input command "sysStateSet"+Enter key in UART, system enters DSM. After system enter DSM, any key input in UART wakeups system. It works well.

But when  input command "sysStateSet"+Enter key in UART, at this time don't release Enter key, still press Enter key. Before or after system enter DSM, release Enter key, then input any key in UART. Sometime system can't wakeup.

I don't understand why UART interrupt can't generate at that time. Receive buffer is full? Receive is disabled? UART clock is disabled? I don't know.

So I want to check GPC_ISRx just before enters DSM. If there is UART interrupt, don't enter DSM. Does it works? How to clear GPC_ISRx status of IRQ58 (UART1)?

During DSM, ARM GIC is disabled.

Thanks,

Miles

Labels (1)
0 Kudos
1 Reply

298 Views
Yuri
NXP Employee
NXP Employee

Hello,

  

    Perhaps the problem takes place since there should not be pending interrupts

before WFI instruction issue.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos