Vivantec GPU does not respond when iMX6Q operates with single core.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vivantec GPU does not respond when iMX6Q operates with single core.

826件の閲覧回数
johnturnur
Contributor III

In SABRESDP(iMX6Q) is there a restriction to keep atleaset 2 core active to use GPU ?


I'm running an OpenGL application on core0. If I shutdown core1,core2,core3 GPU does not respond.


ラベル(3)
タグ(3)
0 件の賞賛
返信
1 返信

612件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, John

     As far as I know, there is no restriction between CORE number and GPU. BTW, when do you shutdown the core1, core2 and core3? Before you lunch GPU app or after? can you try to add "nosmp" or "maxcpus=1" in your uboot command line to let kernel boot up only one core then run the GPU?

0 件の賞賛
返信