Use sd1 as a sd card, open some error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use sd1 as a sd card, open some error

3,851件の閲覧回数
zoechen
Contributor I

Hi FSL,

     I use sd1 to mount our sdcard, when insert our sdcard, system will log:

[mmc3]mmc_wait_for_req: cmd 51

mmc3: Timeout waiting for hardware interrupt.

sdhci: =========== REGISTER DUMP (mmc3)===========

sdhci: Sys addr: 0x1faf6240 | Version:  0x00000002

sdhci: Blk size: 0x00000008 | Blk cnt:  0x00000001

sdhci: Argument: 0x00000000 | Trn mode: 0x00000000

sdhci: Present:  0xfff9820e | Host ctl: 0x00000001

sdhci: Power:    0x0000000d | Blk gap:  0x00000000

sdhci: Wake-up:  0x00000000 | Clock:    0x000010ff

sdhci: Timeout:  0x00000000 | Int stat: 0x00000000

sdhci: Int enab: 0x107f000b | Sig enab: 0x107f000b

sdhci: AC12 err: 0x00000000 | Slot int: 0x00000003

sdhci: Caps:     0x07eb0000 | Caps_1:   0x00000007

sdhci: Cmd:      0x0000333a | Max curr: 0x00ffffff

sdhci: Host ctl2: 0x00000000

sdhci: ===========================================

and I dump the register 0x30 and 0x24, it shows:

0x30: 0x00000001,

0x24: 0xfff9820e.

I send CMD55 before CMD51, it log :

0x30: 0x00000001,

0x24: 0xfff98088.

As your spec said: Read Transfer Active:  A Transfer Complete interrupt is generated when this bit changes to 0(IMX6DQRM, p5484).

So, can you give me some suggestion?

BR,

Zoe

ラベル(2)
0 件の賞賛
返信
6 返答(返信)

3,609件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Zoe

you can test basic SD operations and cmd55 execution with SDK usdhc test

i.MX 6Series Platform SDK  : Bare-metal SDK

also suggest to check SD signals with oscilloscope.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,608件の閲覧回数
zoechen
Contributor I

Hi Igorpadykov,

     I check our SD signals with oscilloscope , the wave of clock and cmd line is right, but after cmd 51 , the data line do not have any wave.

BR,

Zoe

0 件の賞賛
返信

3,608件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

please read part of RM below

CMD51.jpg

~igor

0 件の賞賛
返信

3,608件の閲覧回数
zoechen
Contributor I

Hi Igorpadykov,

     Thanks for you reply first, there is some mistake in my description. It should be ACMD 51, get the value of SCR register.

BR,

Zoe

0 件の賞賛
返信

3,608件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

amcd51 is "application specific" command, not all cards may support it,

1.jpg

~igor

0 件の賞賛
返信

3,608件の閲覧回数
zoechen
Contributor I

Yes, so I test my card in SD2 first, I am sure my card support ACMD51, but I can not use this card in SD1.

BR,

Zoe

0 件の賞賛
返信