OS is NXP Android 9 and soon to be 10
On the camera input side, Whirlpool would like to resize the image down for input into a TensorFlow model and also perform color conversion. I see in the Ref Man Figure 13-18 that the ISI contains a resizer and color conversion blocks.
What API calls or commands can be used to access and control these hardware blocks in the image processing pipeline?