Unused USB_OTG1_OC and USB over-current events

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unused USB_OTG1_OC and USB over-current events

跳至解决方案
1,826 次查看
uthappapj
Contributor II

Hello,

        Our target platform has a i.MX6ULZ SoC running in it. Upon using the USB OTG interface in "host" role for attaching USB digital headsets (e.g., Google Pixel USB-C earbuds) we observed the following Linux kernel error messages being reported:

kern.err kernel: usb usb1-port1: over-current condition
kern.inf kernel: usb 1-1: USB disconnect, device number 2

        After some investigation into the problem, we discovered that on our target platform the USB_OTG1_OC signal had been left unconnected. Also, we came across information in the Linux kernel documentation, that we may have to use the flag "disable-over-current" in the USB OTG1 device node in the device tree specification for our target. Like so:

&usbotg1 {
dr_mode = "otg";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usb_otg1>;
disable-over-current;
status = "okay";
};

        After adding the above change. The USB over-current event stopped appearing. And the USB interface also seems to function normally. We further checked the health of the USB interface using a multi-meter to check if we had wrongly suppressed any real/actual USB over-current situation. But it did not seem to be the case.

        So my query is, whether the solution to use the flag "disable-over-current" the way it's described above, the right way to handle the H/W design we have? Is there anything else that needs to be looked into to ensure that the USB works safely and correctly?

Best regards,

Uthappa

标签 (2)
标记 (4)
0 项奖励
回复
1 解答
1,802 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Uthappa

 

> my query is, whether the solution to use the flag "disable-over-current" the way it's

>described above, the right way to handle the H/W design we have?

 

yes it is correct, in nxp dts file such "disable-over-current" is also used:

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ul-14x14-evk.dtsi?h=...

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,795 次查看
uthappapj
Contributor II

 

        Thank you for confirming this Igor!

-Uthappa

0 项奖励
回复
1,803 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Uthappa

 

> my query is, whether the solution to use the flag "disable-over-current" the way it's

>described above, the right way to handle the H/W design we have?

 

yes it is correct, in nxp dts file such "disable-over-current" is also used:

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ul-14x14-evk.dtsi?h=...

 

Best regards
igor

0 项奖励
回复