Unable to flash code over Device "MIMXRT1052XXXXB".

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to flash code over Device "MIMXRT1052XXXXB".

693 次查看
niket_zope
Contributor III

I have Device "MIMXRT1052XXXXB" whenever is try to connect it via Jlink utility either

JFlash or Jlink commander recieve the following error. It would be very helpful if some can help to resolve the issue.

 

Note: i tried connecting and unlocking the kinetis but it throws an error stating

J-Link>unlock kinetis
Found SWD-DP with ID 0x0BD11477
Unlocking device...ERROR: Read from DP/AP register failed!

 

While flashing the srec it shows this !  

niket_zope_0-1638275289490.png

@jeremyzhou @alex_rodriguez  @Hui_Ma 

 

 

0 项奖励
回复
2 回复数

599 次查看
niket_zope
Contributor III

hi @jeremyzhou , I am using the custom board having MIMXRT1052xxx6B processor connected to it. I am getting the following error when i am trying to read back or even to flash any binary in external flash at location 0x60000000 

 

niket_zope_1-1650602890372.png

 

0 项奖励
回复

686 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Before giving some advice, I'd like to know which board you used for testing.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复