Hi,
I have a 'SABRE for Automotive Infotainment
Based on the i.MX 6 Series' evaluation board.
My onboard CPU is IMX6U which is i.MX 6DualLite processor.
I was trying to run 'ltib' to build the code.
However,when 'LTIB' presented me the CPU (platform) option, I only could find option for IMX6Q or IMX6S, but NOT IMX6U or IMX6D.
What should I choose?
I was told by Freescale technical support to choose 'IMX6S' and 'IMX6dl_sabreauto' as platform in LTIB menu to build U-boot.
However, in the LTIB configuration menu, for 'Choose your board for U-Boot', there are only two options:
'mx6sl_arm2' and 'mx6sl_evk'.
I could NOT find a 'mx6dl_sabreauto' option.
This morning, I tried 'IMX6Q' processor and did find 'mx6dl_sabreauto' option. Should I choose 'IMX6Q' for IMX6U' processor?
Thanks,
Steven
已解决! 转到解答。
Chapter 3 (Building the Linux Platform) of "i.MX_6Solo6DualLite_SABRE-AI_Linux_User's_Guide.pdf" describes
how to build target system for i.MX 6DualLite.
SABRE for Automotive Infotainment Based on the i.MX 6 Series
Chapter 3 (Building the Linux Platform) of "i.MX_6Solo6DualLite_SABRE-AI_Linux_User's_Guide.pdf" describes
how to build target system for i.MX 6DualLite.
SABRE for Automotive Infotainment Based on the i.MX 6 Series
Would you please send me 'L3.0.35_4.1.0_130816_images_MX6.tar.gz'? I could not find it.
Does this package include all the files, u-boot, uImage and rootfs, which are the same as the ones on evaluation board?
Thanks,
Steven
You can download it from here:
Under: Run-Time Software >> Operating System Software - Board Support Packages >> L3.0.35_4.1.0_DEMO_IMAGE_BSP
And yes, it includes everything you ask for.