The problem about IMX6DL GPU when running android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The problem about IMX6DL GPU when running android

2,170件の閲覧回数
pengxingwei
Contributor III

Hi all,

       I develop android_m6.0 on imx6dl sabresd board,when I run a application to dynamic plotting wave by the data thransfering from uart  .But there has waveform caton phenomenon and GPU over drawing,which can discover by the AndroidStudio IDE,How to solve the problem or Is not strong performance of GPU on imx6dl?

ラベル(2)
0 件の賞賛
4 返答(返信)

809件の閲覧回数
pengxingwei
Contributor III

The phenomenon as shown above

0 件の賞賛

809件の閲覧回数
pengxingwei
Contributor III

1.png2.png3.png

0 件の賞賛

809件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi peng

one can try to investigate it, if it caused by ddr bandwidth and using mmdc profiling tool

About MMDC Profiling Tool for i.MX6 

or try latest android releases from link

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

809件の閲覧回数
pengxingwei
Contributor III

Hi igorpadykov,

                     I did the ddr stress through DDR Stress Test tool,and modified the uboot DCD,but The phenomenon is the same as before,

device-2017-11-10-102454.png

0 件の賞賛